Other Parts Discussed in Thread: UCC27714, , LM5146
Dear Expert
Our operation condition is :Input 73~80VDC, output 71.5/20A.
At present, there are some problems with insufficient driver of LM5116. Totem pole was added before. Now we want to add half bridge driver chip UCC27714 between LM5116 and MOS.
Our current schematic diagram is as follows, may I ask how to connect it? Can THE SW pin of LM5116 be disconnected?Or is the SW foot connected to the HS foot of UCC27714?We do not plan to connect the HB of LM5116 to UCC27714, which will have separate power supply.
Please confirm whether this is feasible and how to connect the SW foot?