Hi,
Good day. I hope you are doing well.
Our customer have a technical implementation question.They are using TPS25865-Q1 and they want to know if they can set a different max current limit for the bus out. The connector that they use will get too hot at the max current so they need to limit Ideal max output current is 1.5A. I believe the chip is ~2.4A for each bus, so ~5A total. They need the single output to be 1.5A. Would that be possible?
Looking forward to your inputs. Thank you.
Regards,
Cedrick