This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ25618: [FAQ] Why does ICHG reduce when reaching the maximum duty cycle for the BQ25618, BQ25618E, BQ25619, BQ25611D, BQ25616, BQ25600, BQ25600D, BQ25601, BQ25601D, BQ25606?

Part Number: BQ25618


The charger is basically a step-down DC-DC (buck) converter. It requires the input voltage to be higher than the output voltage with some headroom for normal operations.

  • The maximum duty cycle specification is one of the factors determines the maximum output voltage at a fixed input voltage. Users should avoid maximum duty cycle operations in their applications by setting VINDPM and IINDPM thresholds correctly.
  • Please refer to Extract maximum power from the supply when charging a battery ( https://www.ti.com/lit/an/slyt569/slyt569.pdf ) for the details.