This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ25890: Why does ICHG reduce when reaching the maximum duty cycle for the BQ25890, BQ25890H, BQ25892, BQ25895, BQ25895M, BQ25896, BQ25898, BQ25898D, BQ24190, BQ24192, BQ24195, BQ24195L, BQ24196, BQ24295, BQ24296, BQ24296M, BQ24259?

Part Number: BQ25890


The charger is basically a step-down DC-DC (buck) converter. It requires the input voltage to be higher than the output voltage with some headroom for normal operations.

  • The maximum duty cycle specification is one of the factors determines the maximum output voltage at a fixed input voltage. Users should avoid maximum duty cycle operations in their applications by setting VINDPM and IINDPM thresholds correctly.
  • Please refer to Extract maximum power from the supply when charging a battery (www.ti.com/.../slyt569.pdf) for the details.