In the Dynamic Characteristics section of the specs - page 3 - the timing values are listed as "ns", eg Rise Time = 111 ns. Could this possibly be meant to be "ps"?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the Dynamic Characteristics section of the specs - page 3 - the timing values are listed as "ns", eg Rise Time = 111 ns. Could this possibly be meant to be "ps"?
thank you
Hello Bob,
Thanks for your interest in TI FETs. The CSD17382F4 datasheet is correct. This FET has a relatively large internal gate resistance, 220Ω, typical, which slows down its switching speed. Most of our smaller devices such as FemtoFET and WLP have been optimized for "static" switching applications such as load switch and battery protection where switching speed is not as critical. TI has other FETs in this same footprint with a smaller RG that switch faster. For example, the CSD17381F3 has 23Ω typical RG and its switching speed is much faster.
Best Regards,
John Wallace
TI FET Applications