Have sourcing issue with TPS560430YDBVT and thus plan to drop in LMR50410XDBVR. FYI, I am using TPS560430YDBVT to generate 1.2 and 3.3V from 5V input. From the datasheet, the new part is pin compatible. Not sure if I missed out other parameters.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Have sourcing issue with TPS560430YDBVT and thus plan to drop in LMR50410XDBVR. FYI, I am using TPS560430YDBVT to generate 1.2 and 3.3V from 5V input. From the datasheet, the new part is pin compatible. Not sure if I missed out other parameters.
Hi Ioi,
The main difference is the switching frequency. TPS560430YDBVT is with 2.1MHz while LMR50410XDBVR is 700kHz, which might influence your inductance/capacitance design. You can use Webench to simulate that.
Regards,
Xiaoying