Other Parts Discussed in Thread: TPS61200
Hello,
We are working on a self powered gas valve for water heater application. Thermopile works as a power source only. There is a bulk capacitor for peak current requirement but no primary and secondary battery as backup Thermopile converts thermal energy into electrical energy when heat is provided from gas burner flame. We are looking for a low power DC DC boost converter which converts electrical energy of thermopile 350 to 850mV open circuit (R_teg=3.2 ohm) to 3.3V @ 30-40mA DC voltage to power up micro controllers and other peripherals of the system.
We have explored DC DC boost converter TPS61201 IC. After reading the datasheet and application note, We have below our queries.


If you require more information, please let me know.
Regards,
Ritul