This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQSTUDIO: Explanation of the values in the chemdat.txt file from the installation folder of BQStudio

Part Number: BQSTUDIO

Hello,
I have searched everywhere for this, but I can't find anywhere an explanation of the values from the chemdat.txt file from the installation folder of BQStudio (C:\ti\BatteryManagementStudio\chemistry\chemdat.txt). Vqdis_min, Vqdis_max, SOC_min, SOC_max and Qmax should be clear, but I don't understand what meaning Rhf, Rhf_lo, Rhf_hi and Ra0_charge have. I think Ra0_charge is the resistance at DC current. But even if, to what state-of-charge and temperature? I would be very glad and grateful if someone could explain me the meaning of these values or refer to a document.

With kind regards
Benedikt