Other Parts Discussed in Thread: BQSTUDIO
Hello TI experts,
My customer now tests BQ27542 with Molicel INR18650M35A battery.
they had discharged test, and something happened in this stage.
discharging with 680mA and 3A have no problem.
but if discharging with 2A, when the gauge reaches to 10%, it increases to 16% and then discharged normally.
they tested with 5 batteries, all batteries are same.
I attach the log of each test of discharge. could you check this issue?
MoliCell_3500_DisCharging_2A.xlsx <- it has problem.
i900_MoliCell_3500_DisCharging_680mA.xlsx
i900_MoliCell_3500_DisCharging_3A.xlsx <- These 2 have no problem.
and here is more information,
- They used chemistry ID that already have in bqStudio. (Molicel INR18650M35A - 2481)
- They did not see any special things during learning cycle.
please let me know if you need more information to check this issue. Thanks.
Best regards,
Chase