I am having an issue with the switching regulator not going power save mode. My input is 12v and my load is normally around 20uA, but will go up to around 2.5-3.0 amps when my transmitter turns on. When my load is drawing about 20uA my 12v power supply is at about 350uA. I do have the evaluation board and measured 30uA on the input when my load is at about 20uA. I am not sure what is causing my board to draw so much more current.
I used the same value parts as the EVM board- L1=1uH,C6 =68uF,C1=10uF,C3=22uF, etc. I tried to follow the same pcb layout but due to size restrictions I had to make the ground plane smaller on all the layers. Also, I only have 1 internal ground plane. Another difference is I used ground vias through all the ground planes. Is it possible the layout could cause this, or do i have some component that is incorrect or bad?
The other thing I have noticed is the ripple frequency on the vout(3.3v) line on the EVM is about 156 Hz with a 20uA load. On my pcb it is about 1.3kHz with a 20uA load. In both cases the peak to peak voltage on the ripple is about 40mvpp.
Any suggestions how to troubleshoot this?
Thanks,
Tj