This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073: BQ24073 output current?

Part Number: BQ24073

In BQ24073 datasheet 8page [8.3 Recommended Operating Conditions],

 - Input current, IN pin : 1.5A

 - Current, OUT pin : 4.5A

 - Current, BAT pin (Discharging) : 4.5A

 - Current, BAT pin (Charging) : 1.5A

If both [Current, OUT pin : 4.5A] and[Current, OUT pin : 4.5A] are described, is it possible for both the battery and adapter to use 4.5A load?

The input current(1.5A) includes the system load and the battery charge current.

How can I use the output current up to 4.5A?

Then, after setting the input current(ILIM) to 1.5A, can I use the charging current of 500mA and the load current of 4A?

Thank you.