Hello.
I'm going to design a BMS based on the BQ76952.
However, there is a problem with the availability of the version that communicates over I2C.
The system would communicate with Arduino on the i2c bus.
However, at the moment the available ICs are BQ76952-01 or BQ76952-03 with SPI active. Can these versions be switched to I2C? Do they already have OTP programmed?