This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92391: Programmatic Selection of PWM and current mode transition threshold

Part Number: TPS92391

Section 7.3.8.5 Hybrid Mode of the TPS92391 datasheet, at the bottom of Page 25, states that:

"The PWM and current modes transition threshold can be set at 12.5% or at 0% brightness. The latter selection allows for pure current dimming control mode."

There doesn't appear to be a way to set the transition threshold to these values. Is 12.5% the only value possible when the device is resistor configured to the Hybrid Mode? Similarly, is 0% the only value possible when the device is resistor configured to the Current Dimming Mode?

Am I missing something? It would be desirable to be able to select between these two values programmatically.

Thanks for you help!