Other Parts Discussed in Thread: TPS25947
Hello,
I previously asked about setting I_LIM in the following thread.
In that regard, I would like to ask you a question.
(Question 1)
I am considering setting an I_LIM that exceeds the recommended value of 4A.
However, I plan to set it within the range of 5A, which is the guaranteed design value.
The RILM variability used is ± 1%.
As a reference value, the current limiting accuracy is ± 7.5%.
Considering the above variations, select R_LIM = 440Ω, which maximizes the current limit range as much as possible.
In the calculation, I_LIM (MAX) = 4.98A should be the value considering the variation.
Is it okay to use R_LIM = 440Ω?
Is 440Ω set within the design guarantee?
(Question 2)
In 7.3 Recommended Operating Conditions, C dV / dt is stated as MIN = 3300pF.
Is there a MAX value?
Please let me know any other restrictions or precautions when using this device.
Best regards,
e2e.ti.com/.../tps2595-setting-i_lim-between-4a-and-5a-and-the-resistance-value-in-that-case