Dear Sir/Ms.
My customer wants to design a car light product and intends to use TPS92520. There are some questions in the design. Would you please teach me.
Q1: Can TPS92520 be configured as parallel(Interleave / 2-Phase) output ?
Q2: The customer wants to calculate the power consumption at full load and high temperature. Please tell me the Rds(on) of High side and Low Side when the junction temperature is 125°C.
Q3: The customer's board needs to connect 5~6 TPS92520, need to design the current provided to V5D and V5A. Among them, V5D mentions how much current is needed in the data sheet, but V5A does not. Can you let me know how much current V5A needs? The customer is worried that if the total demand exceeds 150mA, he will design another LDO.
Q4: The data manual states that TPS9250 can output 1.6A, but the current limit of Low side mosfet is 1A. What is the current output of this TPS92520? 0.8A per Chanel?
Best Regards,
Kami Huang