This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43600: Current limit adjustable function device consult

Part Number: LM43600

Hi Team,

Customer wants to choose a buck converter with current limit adjustable function. Below is their circuit demand: Vin_max=30V, Vout=12V, Iout=0.3A. I search on our web but no findings.

Could you pls help us promote a suitable one here? Many thanks.

Best,

Stanley

  • Hi Stanley,

    Can you help advise why your customer needs the current limit adjustable function in buck converter with output current of only 0.3A? Generally our cycle-by-cycle peak/valley current limitation is enough for these applications. Adjustable current limit is typically utilized in high-current applications while the output current should be well monitored. 

    Regards,

    Xiaoying

  • Hi Stanley,

    If customer does need adjustable current limit, you can recommend our buck controller to them.

    If you don't have further question, please help click "resolved" button. Thanks.

    Regards,

    Xiaoying