Hi, support team
My customer has the questions as follow:
1. I need to select a current source chip
current 3A
input voltage 24V
2. What are the methods to adjust current?
I know PWM.
In addition to PWM, what else?
Because PWM needs to be sent by MCU, is there a way to adjust current without MCU.
3. I have used TPS61194 and 8867 chips before.
This chip is a current source.
It is said in the datasheet that it is specially used to drive LED.
Can this chip be used for other loads? Such as a thermoelectric cooler?
4. I need the current source with reverse function. (About question 1)
Is there such a chip?
If not, can I add a full bridge at the output of the current source chip?
Thanks so much.
Best regards,
Yuki