Part Number: TPS2378
Other Parts Discussed in Thread: LM5005,
Dear team
The customer's design is using non-isolated, directly use LM5005 to convert 12V,
1. Does it require opto-coupler?
2. Can T2P directly connected to the CPU?

Many thanks
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Denny,
this is a great question. Since the design is not isolated, then it does not require the optocoupler. I would just ensure the sink and source currents are appropriate for the CPU and the TPS2378. I am not sure if we will need any sort of driver or logic circuit to make the currents appropriate since that is normally done across the optocoupler biasing.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments