This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: about the abs Max SRP-SRN value

Part Number: BQ76930

in BQ769x0 datasheet in page 46, 

However, considering ISCD of 25 A and Abs Max SRP–SRN input of –300 mV, RSNS = 300 mV / 25 A = 7.5 mΩ; the abs Max SRP-SRN is 300mV, why it is 300mV.

in datasheet page 14,  the value is 200mV.