This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM185H-2.5/883Unqualified products

Hi, 

We bought  LM185H-2.5/883  87pcs 

But after we test they are unqualified products.

Here is the result:

30 X-rays are unqualified. Unqualified reason: the bonding cavity of the chip exceeds 1 / 2 of the whole contact area. The specification requires that the PDA is less than or equal to 15%, and the actual PDA is 37%. The PDA has exceeded the standard and the batch is unqualified

But the test are in Chinese. 

Looking forward to your reply