we have generated Boost Converter Using web-bench Design.
which has parameters are as per below.
Vin:- 3.2v Min to 3.7V max
Vout:- 5.3V @5A.
please go through below attached schematic and layout.
we have made some changes as per our calculation which is as per below.
We change the Comp pin(Pin-18 of IC) component as per below.
Designator schematic value updated value
C67 - 27pf-25v 150pf-25v,
C68 - 560pf-25v 1nf-25v,Qty=2,
R55 - 36.5k-25v 20k-25v
L4 - 680nH,12.75A 2.2uH,10A(ASPI-0630LR-2R2M-T15)
All component packages are 0603 packages.
Test case:-
Vin:- 3.7V@5.5A Single Cell
Vout:- 5.3V@ No load
Vout:- 3.7V@3.5 Ohm Resistive Load
so it is not working as per web bench design.
So please suggest the solution for it.
thanks to all in advance.