Other Parts Discussed in Thread: TPS61022, , TPS61230
Hello.
I want to use that boost converter for a gsm/gprs module which has 2A current peaks during transmission (I suppose it's quite standard usecase for such IC). So my incoming voltage will be between 2.8-4.3 V. I'd like to get 4V from this converter. I know about TPS61022, but it's much more expensive here.
Datasheet says that incoming voltage can be from 0.5V to 4.4V, but, the workbench app allows to choose it only less than 3.6V. And all figures in the datasheet covers voltages under 3.6V. Would it work for me?