This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450: Can I use Multiple Ceramic output capacitors instead of single electrolytic.

Part Number: TPS5450

I am designing a 12V to 5V converter using TPS5450 and I was referring the TPS5450 EVM for that. The output capacitor using in the TPS5450 EVM is a 330uF Electrolytic with ESR 35mE.

I am planning to use 7 nos of 47uf  ceramic capacitors along with a 0.01uF ceramic capacitor in my output section of TPS5450.  I hope this will reduce the ESR and will improve the performance of the Buck.

Please let me know if anyone have any concern on this.