This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92380: Thermal question

Part Number: TPS92380

Hi

My customer want to used TPS92380 to replace other LED driver because of thermal issue, they want the IC surface temperature can under 50C.

But seems this EVM have in develop?

Would you have resource to help them run Pspice simulation?

Their work condition is Vin 5~10V, Vout 21V/290mA.

Thanks!

Jeff