Other Parts Discussed in Thread: LM5156
Hi support team,
I am looking for an isolated DC/DC converter with the following specifications.
<Required specifications>
・ Input voltage: 24V (typ) (preferably withstand voltage of max.40V)
・ Output power: 46W or more
・ Output voltage: 54V
・ There is a control terminal that can turn the output on and off.
・ With output overcurrent protection
Is it feasible with the LM5155 Isolated Flyback?
Please let me know if you have a better product.
Regards,
Dice-K