Part Number: LM5050-1
Other Parts Discussed in Thread: TPS25982, TPS2663
A 24V operating voltage for a BLDC motor controller should be secured against overcurrent 6A (10A). The motor controller increases the protected voltage to approx. 26V when braking. A reverse flow protection must therefore be provided. I am thinking of a system consisting of eFuse (TPS25982) and diode controller with external FET (LM5050-1) for the reverse current protection. I would love to have an eFuse that can handle both requirements!
Best Volker