Other Parts Discussed in Thread: LMR50410QEVM
Hi,
Good Day. I have a customer who is working with LMR50410-Q1. Please see below his query for your reference. Thank you very much.
I've integrated two LMR50410Y5FQDBVRQ1 simple switcher circuits into my design and I'm having a problem with them. I used the sample circuit, and set them up with the proper components according to page 17 of the datasheet, one for 5V and one for 3.3V. The input supply voltage is 24V for both switchers. However, my output for the 5V supply is 24V, and the output for the 3.3V supply is around 1.7V, and is in hiccup mode. both circuits are virtually unloaded, save for a 3mA draw on each for an LED, and a few small DACs and Sensors. I anticipate the total draw on each to be about 100mA.
I wanted to simulate in Web Bench, but the webpage said this part wasn't available for Web Bench yet. I fear at this point I might have blown my sensors and ICs on my board with the 24V feed from the 5V supply, but I still need to lock down what happened. I'd appreciate a Monday phone call to help get me back on track.
Best Regards,
Ray Vincent