This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: On / Off using shutdown pin working only to 2.7A

Genius 17175 points
Part Number: TPS1663

Hi all

My customer is using the TPS16632 with Rlim=6K and disconnect works at ~3A ok. (24V, mode=no auto retry).

Running the circuit at 2.8A over several hours works fine.

However they find they cannot switch a load of 2.8A on or off using the shutdown pin.

They had to power down the circuit and reconnect the load.

On off switching at 2.7A works ok.

What could be wrong here ?

Best regards

Ueli