Hi,
a few months ago I created some designs with the following parameters Vin 7-33V Vout=12V Iout 1,5A Temperature .enviroment 60°C and WEBENCH generated the schematic; Now every time that I try to create a new design I get the following error: "Design update failed - OpVal table param temperature> 150 ° C.
How I can generate the schematic?
My request is Vin=8-32V Vout=12V Iout=1 to 1,5A / Tenviroment 60 to 70°C / Highest possible frequency
Thanks