Other Parts Discussed in Thread: UCC2897A
Hello,
I am considering the following two specifications for an insulated power supply.
For both specifications, I want to create a circuit on the same device.
I think the UCC28600 meets the requirements, but please let us know what you think.
(Specification 1)
Input voltage: DC24Vtyp (DC18V-30V)
Output voltage: DC12V
Output current: 5.1A (Max 6.1A)
Efficiency: 85% or more
(Specification 2)
Input voltage: AC85V to 264V
Output voltage: DC12V
Output current: 5.1A (Max 6.1A)
Efficiency: 85% or more
Best regards,