Hi Sir,
We encountered a problem when using TPS546D24A, that is, when the load current is greater than 10A, there is no output. By carefully checking our design, we believe that the protection is triggered when the load current is 10A, which cause no output. Can u help us to check the cause of this problem?
The below is the schematic and PCB layout diagram, hope it can do some help for the problem analysis.
Thanks,
Best Regards