I use BQ78350 as my coulometer, Lithium battery 14 string, battery configurations 64Ahr. the cell aging study unsuccessful.
the data flash as attachment, please give us some advise, thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use BQ78350 as my coulometer, Lithium battery 14 string, battery configurations 64Ahr. the cell aging study unsuccessful.
the data flash as attachment, please give us some advise, thanks!
Hi,
Can you describe more what you mean by the cell aging study is unsuccessful? I am not sure I understand.
If you can provide a log file and a description of the behavior it would be helpful. I noticed from your register settings, that the gauging parameters are all set to the default values. If you want to set up the device for accurate gauging, you need to go through the steps in the Gas Gauging section of the "Using the BQ78350-R1" application document.
Best regards,
Matt
Understood. For this, you need to go through the steps in the Gas Gauging section of the Using the BQ78350-R1 document: https://www.ti.com/lit/an/slua924/slua924.pdf The Learned Full Charge Capacity will be updated after a full discharge cycle. This value will decrease as the capacity decreases as the battery ages.