Other Parts Discussed in Thread: TPS2062
If my voltage source is 5V,5A then during short circuit entire 5A will flow into load, how TPS2066C responds to short circuit condition. |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If my voltage source is 5V,5A then during short circuit entire 5A will flow into load, how TPS2066C responds to short circuit condition. |
Hi Pavaman,
1. Figure 9 is in current limit condition.
2. For short circuit condition, you can refer to figure 16. It will thermal cycle.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.
Hi
Fig7, Fig 8 When enabled output took 4mSec after Vin > 3V,
But in loaded condition in Fig 9 output responded in 1mSec. Why so ? Is it because of load in Fig 7 load is 1A and Fig 9 load is 2.5A.
i am little confused for higher loads the out responds in 1mSec. generally it should be reverse ? AM i right. ?
In Fig 13 no output is shown in graph where by load is 2A. which is max for tps2062. Output should go High and then fall right ? may be in 4mSec.pls correct me.
in Fig 11, output short there is not Vout , But when Iout=0 output is high. something is missing in me?
Pavaman,
1. For Fig7 and Fig9, you can refer to the position of arrow. That's the position to calculate the period. They are same.
2. For Fig13, it's enabled into short. It means that output should always be 0.
3. Short to GND, of course to be 0V.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.