This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24074: Charger IC burnout

Part Number: BQ24074

Hi TI experts,

My company is mass-producing boards with BQ24074 applied.

The BQ24074 burnout or no output symptom occurred in around 400 out of a total of 5000 products.

Please check the circuit design and give me some guide for solve this problem.

The circuit setting is as follows.

1. Vin : 5V

2. symptom : Device Burn-out or no Output.

3. OUT is not used for system power 

    VBAT is directly connected to system power lane and the system use over 20A (current) at battery side