Hi,
I use DCDC LM43602 and have next have DCDC Requirements:
1. Very wide Vin – from 5.5V to 29.3V
2. Output Current – min 30mA to max. 800mA
3. Vout is 4.37V
I used TI Webench
And, calculated by formulas from Datasheet LM43602PWPR
I don’t like that TI Webench recommended to use inductor 15uH for switching freq. 440kHz
Calculation point that:
- for min Vin 5.5V it should be less than 15uH -----12.37uH
- for 30V more than 15uH ----- 26.41uH
Could you send your recommendation for inductor choice and switching freq.?
I understand Input Voltage too wide, but I can get compromise in efficiency
Best regards,
Anatoli