This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3411R070: Applicaton report SNOAA15

Part Number: LMG3411R070


Hi all

Would you mind if we ask LMG3411R070?

There is the applicaton report SNOAA15 which is "Overcurrent Protection in High-Density GaN Power Designs".
https://www.ti.com/lit/pdf/snoaa15

There is the description on the application as follows;
"During cycle-by-cycle operation, after the current reaches the upper limit with the PWM input still high,
 the load current can flow through the third quadrant of the other FET of a half-bridge with no synchronous rectification.
 The extra high negative voltage drop (–6 V to –8 V) from drain to source could lead to high third quadrant loss, similar to dead time loss but with much longer time. 
 Therefore, it is critical to design the control scheme to make sure the number of switching cycles in cycle-by-cycle mode is limited, 
 or to change PWM input based on the fault signal to shorten the time in third quadrant conduction mode of the power stage."

We could not understand the word "third quadrant" and "third quadrant loss".
Could you give us these meanings?

Kind regards,

Hirotaka Matsumoto

  • Hi Hirotaka, thanks for your question. 

    The term "third quadrant" refers to the conduction of current through the GaN FET in the reverse direction - that is, from source to drain. For a MOSFET, third quadrant operation occurs when the current flows from the source to the drain terminal through the body diode or the channel. Although GaN FETs have no body diode, the symmetry of the device helps conduct in the third quadrant with diode-like behavior. This reverse current conduction is enabled when Vgd = Vgs + Vsd > Vth. 

    Third quadrant loss occurs as a result of the high Vds drop when the reverse current is flowing through the device. 

    Please see Sections 2 and 3 of this application report for more in-depth information on the third quadrant operation of GaN devices.  

    Best Regards,

    John