Other Parts Discussed in Thread: UCC28910, UCC28910FBEVM-526,
My customer request a PWM controller with integrated FET, the power requirement is 2W; is there any suitable device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer request a PWM controller with integrated FET, the power requirement is 2W; is there any suitable device?
Hi, Yachne:
UCC28910 would be a solution to you.
Compare to UCC28740, UCC28910 is PSR control with integrated MOSFET and provides CV/CC function. The max power rating shows on page 3 in its datasheet. UCC28910 could support max 6W output as full range input. UCC28910FBEVM-526 would be a reference for its performance.
However, SSR has better dynamic response and CC/CV accuracy. Thus, is there any specific system request for this one?
Best regards.
Wesley