This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76942: Communication between bq76942 and bqStudio

Part Number: BQ76942
Other Parts Discussed in Thread: BQSTUDIO, , MSP430FR2355

Hi

Does anyone know how the bq76942 communicate with bqStudio on the bq76942EMV evaluation board? Does the chip communicate directly with bqStuido or does he communicate over the MSP430?
If the chip communicate over the MSP430 is the source code of the msp430 (used on bq76942EMV) available?

Thx for the help!

  • Hi Pascal,

    The BQ76942 communicates through the MSP430 on the board. We do not have source code to share for the MSP430 unfortunately.

    I do have example code to share for a couple of different microcontrollers to work with the BQ76942 if you need. This would not interface to BQStudio though.

    Best regards,

    Matt

  • Hi Matt

    Thank for your answer! Where can I find this example code for the different microcontroller to work with BQ76942? Would be nice to look at it even though i doesn't enable a connection to bqStudio. 

    Kind regards,

    Pascal 

  • Hi Pascal,

    See the code attached. There is a header file along with two different main files - one is for an MSP430FR2355 and one is using an ARM based MCU.

    BQ769x2Header.h

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2021, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*//* USER CODE BEGIN Header */
    /**
      ******************************************************************************
      * @file           : main.c
      * @brief          : Main program body 
      * (Non-USER sections generated from STM32CubeMX software)
      ******************************************************************************
      * @attention
      *
      * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
      * All rights reserved.</center></h2>
      *
      * This software component is licensed by ST under BSD 3-Clause license,
      * the "License"; You may not use this file except in compliance with the
      * License. You may obtain a copy of the License at:
      *                        opensource.org/licenses/BSD-3-Clause
      *
      ******************************************************************************
      */
    //  BQ76952EVM demo code for STM32 NUCLEO-F103RB + BQ76952EVM 
    //
    //  Connection description: The I2C SCL and SDA pins are the only pin connections required between the
    //  NUCLEO board and the BQ76952EVM for this demo code. Also a ground connection should be made between the 2 boards.
    //  The ALERT, RST_SHUT, and DFETOFF pins are also configured on the MCU and can be used as shown.
    //
    //                                     /|\ /|\ 
    //                   STM32             5k |
    //                 -----------------    |  5k
    //                |             PB8 |---+---|-- I2C Clock (SCL)
    //                |                 |       |
    //                |		        PB9 |-------+-- I2C Data (SDA)
    //                |                 |
    //     DFETOFF ---| PA8             |
    //                |                 |
    //   RST_SHUT  ---| PA9        		|--- Green LED
    //                |                 |
    //      ALERT  ---|	PA10            |
    //                |                 |
    
    
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    #include <stdio.h>
    #include "BQ769x2Header.h"
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    #define DEV_ADDR  0x10  // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address
    #define CRC_Mode 0  // 0 for disabled, 1 for enabled
    #define MAX_BUFFER_SIZE 10
    #define R 0 // Read; Used in DirectCommands and Subcommands functions
    #define W 1 // Write; Used in DirectCommands and Subcommands functions
    #define W2 2 // Write data with two bytes; Used in Subcommands function
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    I2C_HandleTypeDef hi2c1;
    
    TIM_HandleTypeDef htim1;
    
    UART_HandleTypeDef huart2;
    
    /* USER CODE BEGIN PV */
    uint8_t RX_data [2] = {0x00, 0x00}; // used in several functions to store data read from BQ769x2
    uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 
    	0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    	//used in Subcommands read function
    // Global Variables for cell voltages, temperatures, Stack voltage, PACK Pin voltage, LD Pin voltage, CC2 current
    uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    float Temperature [3] = {0,0,0};
    uint16_t Stack_Voltage = 0x00;
    uint16_t Pack_Voltage = 0x00;
    uint16_t LD_Voltage = 0x00;
    uint16_t Pack_Current = 0x00;
    
    uint16_t AlarmBits = 0x00;
    uint8_t value_SafetyStatusA;  // Safety Status Register A
    uint8_t value_SafetyStatusB;  // Safety Status Register B
    uint8_t value_SafetyStatusC;  // Safety Status Register C
    uint8_t value_PFStatusA;   // Permanent Fail Status Register A
    uint8_t value_PFStatusB;   // Permanent Fail Status Register B
    uint8_t value_PFStatusC;   // Permanent Fail Status Register C
    uint8_t FET_Status;  // FET Status register contents  - Shows states of FETs
    uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
    
    uint8_t	UV_Fault = 0;   // under-voltage fault state
    uint8_t	OV_Fault = 0;   // over-voltage fault state
    uint8_t	SCD_Fault = 0;  // short-circuit fault state
    uint8_t	OCD_Fault = 0;  // over-current fault state
    uint8_t ProtectionsTriggered = 0; // Set to 1 if any protection triggers
    
    uint8_t LD_ON = 0;	// Load Detect status bit
    uint8_t DSG = 0;   // discharge FET state
    uint8_t CHG = 0;   // charge FET state
    uint8_t PCHG = 0;  // pre-charge FET state
    uint8_t PDSG = 0;  // pre-discharge FET state
    
    uint32_t AccumulatedCharge_Int; // in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Frac;// in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Time;// in BQ769x2_READPASSQ func
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_I2C1_Init(void);
    static void MX_USART2_UART_Init(void);
    static void MX_TIM1_Init(void);
    /* USER CODE BEGIN PFP */
    void delayUS(uint32_t us) {   // Sets the delay in microseconds.
    	__HAL_TIM_SET_COUNTER(&htim1,0);  // set the counter value a 0
    	while (__HAL_TIM_GET_COUNTER(&htim1) < us);  // wait for the counter to reach the us input in the parameter
    }
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    unsigned char Checksum(unsigned char *ptr, unsigned char len)
    // Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.	
    {
    	unsigned char i;
    	unsigned char checksum = 0;
    
    	for(i=0; i<len; i++)
    		checksum += ptr[i];
    
    	checksum = 0xff & ~checksum;
    
    	return(checksum);
    }
    
    unsigned char CRC8(unsigned char *ptr, unsigned char len)
    //Calculates CRC8 for passed bytes. Used in i2c read and write functions 
    {
    	unsigned char i;
    	unsigned char crc=0;
    	while(len--!=0)
    	{
    		for(i=0x80; i!=0; i/=2)
    		{
    			if((crc & 0x80) != 0)
    			{
    				crc *= 2;
    				crc ^= 0x107;
    			}
    			else
    				crc *= 2;
    
    			if((*ptr & i)!=0)
    				crc ^= 0x107;
    		}
    		ptr++;
    	}
    	return(crc);
    }
    
    void I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		crc_count = count * 2;
    		uint8_t crc1stByteBuffer [3] = {0x10, reg_addr, reg_data[0]};
    		unsigned int j;
    		unsigned int i;
    		uint8_t temp_crc_buffer [3];
    
    		TX_Buffer[0] = reg_data[0];
    		TX_Buffer[1] = CRC8(crc1stByteBuffer,3);
    
    		j = 2;
    		for(i=1; i<count; i++)
    		{
    			TX_Buffer[j] = reg_data[i];
    			j = j + 1;
    			temp_crc_buffer[0] = reg_data[i];
    			TX_Buffer[j] = CRC8(temp_crc_buffer,1);
    			j = j + 1;
    		}
    		HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, TX_Buffer, crc_count, 1000);
    	}
    #else 
    	HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    }
    
    int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	unsigned int RX_CRC_Fail = 0;  // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
    	uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    		crc_count = count * 2;
    		unsigned int j;
    		unsigned int i;
    		unsigned char CRCc = 0;
    		uint8_t temp_crc_buffer [3];
    
    		HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
    		uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
    		CRCc = CRC8(crc1stByteBuffer,4);
    		if (CRCc != ReceiveBuffer[1])
    		{
    			RX_CRC_Fail += 1;
    		}
    		RX_Buffer[0] = ReceiveBuffer[0];
    
    		j = 2;
    		for (i=1; i<count; i++)
    		{
    			RX_Buffer[i] = ReceiveBuffer[j];
    			temp_crc_buffer[0] = ReceiveBuffer[j];
    			j = j + 1;
    			CRCc = CRC8(temp_crc_buffer,1);
    			if (CRCc != ReceiveBuffer[j])
    				RX_CRC_Fail += 1;
    			j = j + 1;
    		}
    		CopyArray(RX_Buffer, reg_data, crc_count);
    	}
    #else
    	HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    	return 0;
    }
    
    void BQ769x2_SetRegister(uint16_t reg_addr, uint32_t reg_data, uint8_t datalen)
    {
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    	uint8_t TX_RegData[6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    
    	//TX_RegData in little endian format
    	TX_RegData[0] = reg_addr & 0xff; 
    	TX_RegData[1] = (reg_addr >> 8) & 0xff;
    	TX_RegData[2] = reg_data & 0xff; //1st byte of data
    
    	switch(datalen)
        {
    		case 1: //1 byte datalength
          		I2C_WriteReg(0x3E, TX_RegData, 3);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 3); 
    			TX_Buffer[1] = 0x05; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 2: //2 byte datalength
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 4);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 4); 
    			TX_Buffer[1] = 0x06; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 4: //4 byte datalength, Only used for CCGain and Capacity Gain
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			TX_RegData[4] = (reg_data >> 16) & 0xff;
    			TX_RegData[5] = (reg_data >> 24) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 6);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 6); 
    			TX_Buffer[1] = 0x08; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
        }
    }
    
    void CommandSubcommands(uint16_t command) //For Command only Subcommands
    // See the TRM or the BQ76952 header file for a full list of Command-only subcommands
    {	//For DEEPSLEEP/SHUTDOWN subcommand you will need to call this function twice consecutively
    	
    	uint8_t TX_Reg[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff;
    
    	I2C_WriteReg(0x3E,TX_Reg,2); 
    	delayUS(2000);
    }
    
    void Subcommands(uint16_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Subcommands
    {
    	//security keys and Manu_data writes dont work with this function (reading these commands works)
    	//max readback size is 32 bytes i.e. DASTATUS, CUV/COV snapshot
    	uint8_t TX_Reg[4] = {0x00, 0x00, 0x00, 0x00};
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff; 
    
    	if (type == R) {//read
    		I2C_WriteReg(0x3E,TX_Reg,2);
    		delayUS(2000);
    		I2C_ReadReg(0x40, RX_32Byte, 32); //RX_32Byte is a global variable
    	}
    	else if (type == W) {
    		//FET_Control, REG12_Control
    		TX_Reg[2] = data & 0xff; 
    		I2C_WriteReg(0x3E,TX_Reg,3);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 3);
    		TX_Buffer[1] = 0x05; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000); 
    	}
    	else if (type == W2){ //write data with 2 bytes
    		//CB_Active_Cells, CB_SET_LVL
    		TX_Reg[2] = data & 0xff; 
    		TX_Reg[3] = (data >> 8) & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg,4);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 4); 
    		TX_Buffer[1] = 0x06; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000); 
    	}
    }
    
    void DirectCommands(uint8_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Direct Commands
    {	//type: R = read, W = write
    	uint8_t TX_data[2] = {0x00, 0x00};
    
    	//little endian format
    	TX_data[0] = data & 0xff;
    	TX_data[1] = (data >> 8) & 0xff;
    
    	if (type == R) {//Read
    		I2C_ReadReg(command, RX_data, 2); //RX_data is a global variable
    		delayUS(2000);
    	}
    	if (type == W) {//write
        //Control_status, alarm_status, alarm_enable all 2 bytes long
    		I2C_WriteReg(command,TX_data,2);
    		delayUS(2000);
    	}
    }
    
    void BQ769x2_Init() {
    	// Configures all parameters in device RAM
    
    	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
    	// See TRM for full description of CONFIG_UPDATE mode
    	CommandSubcommands(SET_CFGUPDATE);
    
    	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
    	// programmed for the change to take effect. All of the RAM registers are described in detail in the BQ769x2 TRM.
    	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
    	// a full description of the register and the bits will pop up on the screen.
    
    	// 'Power Config' - 0x9234 = 0x2D80
    	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
      	// Set wake speed bits to 00 for best performance
    	BQ769x2_SetRegister(PowerConfig, 0x2D80, 2);
    
    	// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
    	BQ769x2_SetRegister(REG0Config, 0x01, 1);
    
    	// 'REG12 Config' - Enable REG1 with 3.3V output (0x0D for 3.3V, 0x0F for 5V)
    	BQ769x2_SetRegister(REG12Config, 0x0D, 1);
    
    	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
    	BQ769x2_SetRegister(DFETOFFPinConfig, 0x42, 1);
    
    	// Set up ALERT Pin - 0x92FC = 0x2A
    	// This configures the ALERT pin to drive high (REG1 voltage) when enabled.
    	// The ALERT pin can be used as an interrupt to the MCU when a protection has triggered or new measurements are available
    	BQ769x2_SetRegister(ALERTPinConfig, 0x2A, 1);
    
    	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07
    	BQ769x2_SetRegister(TS1Config, 0x07, 1);
    
    	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F
    	BQ769x2_SetRegister(TS3Config, 0x0F, 1);
    
    	// Set HDQ to measure Cell Temperature - 0x9300 = 0x07
    	BQ769x2_SetRegister(HDQPinConfig, 0x07, 1);
    
    	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000; Writing 0x0000 sets the default of 16 cells
    	BQ769x2_SetRegister(VCellMode, 0x0000, 2);
    
    	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC
    	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
    	// COV (over-voltage), CUV (under-voltage)
    	BQ769x2_SetRegister(EnabledProtectionsA, 0xBC, 1);
    
    	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7
    	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
    	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
    	BQ769x2_SetRegister(EnabledProtectionsB, 0xF7, 1);
    
    	// 'Default Alarm Mask' - 0x..82 Enables the FullScan and ADScan bits, default value = 0xF800
    	BQ769x2_SetRegister(DefaultAlarmMask, 0xF882, 2);
    
    	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
    	// Also see "Cell Balancing with BQ769x2 Battery Monitors" document on ti.com
    	BQ769x2_SetRegister(BalancingConfiguration, 0x03, 1);
    
    	// Set up CUV (under-voltage) Threshold - 0x9275 = 0x31 (2479 mV)
    	// CUV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(CUVThreshold, 0x31, 1);
    
    	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
    	// COV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(COVThreshold, 0x55, 1);
    
    	// Set up OCC (over-current in charge) Threshold - 0x9280 = 0x05 (10 mV = 10A across 1mOhm sense resistor) Units in 2mV
    	BQ769x2_SetRegister(OCCThreshold, 0x05, 1);
    
    	// Set up OCD1 Threshold - 0x9282 = 0x0A (20 mV = 20A across 1mOhm sense resistor) units of 2mV
    	BQ769x2_SetRegister(OCD1Threshold, 0x0A, 1);
    
    	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)  0x05=100mV
    	BQ769x2_SetRegister(SCDThreshold, 0x05, 1);
    
    	// Set up SCD Delay - 0x9287 = 0x03 (30 us) Enabled with a delay of (value - 1) * 15 µs; min value of 1    
    	BQ769x2_SetRegister(SCDDelay, 0x03, 1);
    
    	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
    	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
    	BQ769x2_SetRegister(SCDLLatchLimit, 0x01, 1);
    
    	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
    	CommandSubcommands(EXIT_CFGUPDATE);
    }
    
    //  ********************************* FET Control Commands  ***************************************
    
    void BQ769x2_BOTHOFF () {
    	// Disables all FETs using the DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);  // DFETOFF pin (BOTHOFF) set high
    }
    
    void BQ769x2_RESET_BOTHOFF () {
    	// Resets DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
    }
    
    void BQ769x2_ReadFETStatus() { 
    	// Read FET Status to see which FETs are enabled
    	DirectCommands(FETStatus, 0x00, R);
    	FET_Status = (RX_data[1]*256 + RX_data[0]);
    	DSG = ((0x4 & RX_data[0])>>2);// discharge FET state
      	CHG = (0x1 & RX_data[0]);// charge FET state
      	PCHG = ((0x2 & RX_data[0])>>1);// pre-charge FET state
      	PDSG = ((0x8 & RX_data[0])>>3);// pre-discharge FET state
    }
    
    // ********************************* End of FET Control Commands *********************************
    
    // ********************************* BQ769x2 Power Commands   *****************************************
    
    void BQ769x2_ShutdownPin() {
    	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function	
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);  // Sets RST_SHUT pin
    }
    
    void BQ769x2_ReleaseShutdownPin() {
    	// Releases the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function	
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // Resets RST_SHUT pin
    }
    
    // ********************************* End of BQ769x2 Power Commands   *****************************************
    
    
    // ********************************* BQ769x2 Status and Fault Commands   *****************************************
    
    uint16_t BQ769x2_ReadAlarmStatus() { 
    	// Read this register to find out why the ALERT pin was asserted
    	DirectCommands(AlarmStatus, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);
    }
    
    void BQ769x2_ReadSafetyStatus() { //good example functions
    	// Read Safety Status A/B/C and find which bits are set
    	// This shows which primary protections have been triggered
    	DirectCommands(SafetyStatusA, 0x00, R);
    	value_SafetyStatusA = (RX_data[1]*256 + RX_data[0]);
    	//Example Fault Flags
    	UV_Fault = ((0x4 & RX_data[0])>>2); 
    	OV_Fault = ((0x8 & RX_data[0])>>3);
    	SCD_Fault = ((0x8 & RX_data[1])>>3);
    	OCD_Fault = ((0x2 & RX_data[1])>>1);
    	DirectCommands(SafetyStatusB, 0x00, R);
    	value_SafetyStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(SafetyStatusC, 0x00, R);
    	value_SafetyStatusC = (RX_data[1]*256 + RX_data[0]);
    	if ((value_SafetyStatusA + value_SafetyStatusB + value_SafetyStatusC) > 1) {
    		ProtectionsTriggered = 1; }
    	else {
    		ProtectionsTriggered = 0; }
    }
    
    void BQ769x2_ReadPFStatus() {
    	// Read Permanent Fail Status A/B/C and find which bits are set
    	// This shows which permanent failures have been triggered
    	DirectCommands(PFStatusA, 0x00, R);
    	value_PFStatusA = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusB, 0x00, R);
    	value_PFStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusC, 0x00, R);
    	value_PFStatusC = (RX_data[1]*256 + RX_data[0]);
    }
    
    // ********************************* End of BQ769x2 Status and Fault Commands   *****************************************
    
    
    // ********************************* BQ769x2 Measurement Commands   *****************************************
    
    
    uint16_t BQ769x2_ReadVoltage(uint8_t command)
    // This function can be used to read a specific cell voltage or stack / pack / LD voltage
    {
    	//RX_data is global var
    	DirectCommands(command, 0x00, R);
    	if(command >= Cell1Voltage && command <= Cell16Voltage) {//Cells 1 through 16 (0x14 to 0x32)
    		return (RX_data[1]*256 + RX_data[0]); //voltage is reported in mV
    	}
    	else {//stack, Pack, LD
    		return 10 * (RX_data[1]*256 + RX_data[0]); //voltage is reported in 0.01V units
    	}
    
    }
    void BQ769x2_ReadAllVoltages()
    // Reads all cell voltages, Stack voltage, PACK pin voltage, and LD pin voltage
    {
      int cellvoltageholder = Cell1Voltage; //Cell1Voltage is 0x14
      for (int x = 0; x < 16; x++){//Reads all cell voltages
        CellVoltage[x] = BQ769x2_ReadVoltage(cellvoltageholder);
        cellvoltageholder = cellvoltageholder + 2;
      }
      Stack_Voltage = BQ769x2_ReadVoltage(StackVoltage);
      Pack_Voltage = BQ769x2_ReadVoltage(PACKPinVoltage);
      LD_Voltage = BQ769x2_ReadVoltage(LDPinVoltage);
    }
    
    uint16_t BQ769x2_ReadCurrent() 
    // Reads PACK current 
    {
    	DirectCommands(CC2Current, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);  // current is reported in mA
    }
    
    float BQ769x2_ReadTemperature(uint8_t command) 
    {
    	DirectCommands(command, 0x00, R);
    	//RX_data is a global var
    	return (0.1 * (float)(RX_data[1]*256 + RX_data[0])) - 273.15;  // converts from 0.1K to Celcius
    }
    
    void BQ769x2_ReadPassQ(){ // Read Accumulated Charge and Time from DASTATUS6 
    	Subcommands(DASTATUS6, 0x00, R);
    	AccumulatedCharge_Int = ((RX_32Byte[3]<<24) + (RX_32Byte[2]<<16) + (RX_32Byte[1]<<8) + RX_32Byte[0]); //Bytes 0-3
    	AccumulatedCharge_Frac = ((RX_32Byte[7]<<24) + (RX_32Byte[6]<<16) + (RX_32Byte[5]<<8) + RX_32Byte[4]); //Bytes 4-7
    	AccumulatedCharge_Time = ((RX_32Byte[11]<<24) + (RX_32Byte[10]<<16) + (RX_32Byte[9]<<8) + RX_32Byte[8]); //Bytes 8-11
    }
    
    // ********************************* End of BQ769x2 Measurement Commands   *****************************************
    
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    /* USER CODE END 0 */
    
    /**
      * @brief  The application entry point.
      * @retval int
      */
    int main(void)
    {
      /* USER CODE BEGIN 1 */
    
      /* USER CODE END 1 */
    
      /* MCU Configuration--------------------------------------------------------*/
    
      /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
      	HAL_Init();
    
      /* USER CODE BEGIN Init */
    
      /* USER CODE END Init */
    
      /* Configure the system clock */
      	SystemClock_Config();
    
      /* USER CODE BEGIN SysInit */
    
      /* USER CODE END SysInit */
    
      /* Initialize all configured peripherals */
      	MX_GPIO_Init();
      	MX_I2C1_Init();
      	MX_USART2_UART_Init();
      	MX_TIM1_Init();
      /* USER CODE BEGIN 2 */
    	// Start timer
    	HAL_TIM_Base_Start(&htim1);
    
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // RST_SHUT pin set low
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
      	delayUS(10000);
    
    	CommandSubcommands(BQ769x2_RESET);  // Resets the BQ769x2 registers
    	delayUS(60000);
    	BQ769x2_Init();  // Configure all of the BQ769x2 register settings
    	delayUS(10000);
    	CommandSubcommands(FET_ENABLE); // Enable the CHG and DSG FETs
    	delayUS(10000);
    	CommandSubcommands(SLEEP_DISABLE); // Sleep mode is enabled by default. For this example, Sleep is disabled to 
    									   // demonstrate full-speed measurements in Normal mode. 
    
    	delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000);  //wait to start measurements after FETs close
    
      /* USER CODE END 2 */
    
      /* Infinite loop */
      /* USER CODE BEGIN WHILE */
      while (1)
      {
        /* USER CODE END WHILE */
    
        /* USER CODE BEGIN 3 */
    	
        //Reads Cell, Stack, Pack, LD Voltages, Pack Current and TS1/TS3 Temperatures in a loop
    	//This basic example polls the Alarm Status register to see if protections have triggered or new measurements are ready
    	//The ALERT pin can also be used as an interrupt to the microcontroller for fastest response time instead of polling
    	//In this example the LED on the microcontroller board will be turned on to indicate a protection has triggered and will 
    	//be turned off if the protection condition has cleared.
    
    		AlarmBits = BQ769x2_ReadAlarmStatus();
    		if (AlarmBits & 0x80) {  // Check if FULLSCAN is complete. If set, new measurements are available
          		BQ769x2_ReadAllVoltages();
          		Pack_Current = BQ769x2_ReadCurrent();
          		Temperature[0] = BQ769x2_ReadTemperature(TS1Temperature);
          		Temperature[1] = BQ769x2_ReadTemperature(TS3Temperature);
    			DirectCommands(AlarmStatus, 0x0080, W);  // Clear the FULLSCAN bit
    		}
    				
    		if (AlarmBits & 0xC000) {  // If Safety Status bits are showing in AlarmStatus register
    			BQ769x2_ReadSafetyStatus(); // Read the Safety Status registers to find which protections have triggered
    			if (ProtectionsTriggered & 1) {
    				HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_SET); }// Turn on the LED to indicate Protection has triggered
    				DirectCommands(AlarmStatus, 0xF800, W); // Clear the Safety Status Alarm bits.
    			}
    		else
    		{
    			if (ProtectionsTriggered & 1) {
    				BQ769x2_ReadSafetyStatus();
    				if (!(ProtectionsTriggered & 1)) 
    				{
    					HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_RESET);
    				} 
    			} // Turn off the LED if Safety Status has cleared which means the protection condition is no longer present
    		}
    		delayUS(20000);  // repeat loop every 20 ms
      }
      /* USER CODE END 3 */
    }
    
    /**
      * @brief System Clock Configuration
      * @retval None
      */
    void SystemClock_Config(void)
    {
      RCC_OscInitTypeDef RCC_OscInitStruct = {0};
      RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
      /** Initializes the RCC Oscillators according to the specified parameters
      * in the RCC_OscInitTypeDef structure.
      */
      RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
      RCC_OscInitStruct.HSEState = RCC_HSE_ON;
      RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
      RCC_OscInitStruct.HSIState = RCC_HSI_ON;
      RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
      RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
      RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;
      if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
      {
        Error_Handler();
      }
      /** Initializes the CPU, AHB and APB buses clocks
      */
      RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                                  |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
      RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
      RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
      RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
      RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
      if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
      {
        Error_Handler();
      }
    }
    
    /**
      * @brief I2C1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_I2C1_Init(void)
    {
    
      /* USER CODE BEGIN I2C1_Init 0 */
    
      /* USER CODE END I2C1_Init 0 */
    
      /* USER CODE BEGIN I2C1_Init 1 */
    
      /* USER CODE END I2C1_Init 1 */
      hi2c1.Instance = I2C1;
      hi2c1.Init.ClockSpeed = 400000;
      hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
      hi2c1.Init.OwnAddress1 = 0;
      hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
      hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
      hi2c1.Init.OwnAddress2 = 0;
      hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
      hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
      if (HAL_I2C_Init(&hi2c1) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN I2C1_Init 2 */
    
      /* USER CODE END I2C1_Init 2 */
    
    }
    
    /**
      * @brief TIM1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_TIM1_Init(void)
    {
    
      /* USER CODE BEGIN TIM1_Init 0 */
    
      /* USER CODE END TIM1_Init 0 */
    
      TIM_ClockConfigTypeDef sClockSourceConfig = {0};
      TIM_MasterConfigTypeDef sMasterConfig = {0};
    
      /* USER CODE BEGIN TIM1_Init 1 */
    
      /* USER CODE END TIM1_Init 1 */
      htim1.Instance = TIM1;
      htim1.Init.Prescaler = 63;
      htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
      htim1.Init.Period = 65535;
      htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
      htim1.Init.RepetitionCounter = 0;
      htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
      if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
      {
        Error_Handler();
      }
      sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
      if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
      {
        Error_Handler();
      }
      sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
      sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
      if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN TIM1_Init 2 */
    
      /* USER CODE END TIM1_Init 2 */
    
    }
    
    /**
      * @brief USART2 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_USART2_UART_Init(void)
    {
    
      /* USER CODE BEGIN USART2_Init 0 */
    
      /* USER CODE END USART2_Init 0 */
    
      /* USER CODE BEGIN USART2_Init 1 */
    
      /* USER CODE END USART2_Init 1 */
      huart2.Instance = USART2;
      huart2.Init.BaudRate = 115200;
      huart2.Init.WordLength = UART_WORDLENGTH_8B;
      huart2.Init.StopBits = UART_STOPBITS_1;
      huart2.Init.Parity = UART_PARITY_NONE;
      huart2.Init.Mode = UART_MODE_TX_RX;
      huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
      huart2.Init.OverSampling = UART_OVERSAMPLING_16;
      if (HAL_UART_Init(&huart2) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN USART2_Init 2 */
    
      /* USER CODE END USART2_Init 2 */
    
    }
    
    /**
      * @brief GPIO Initialization Function
      * @param None
      * @retval None
      */
    static void MX_GPIO_Init(void)
    {
      GPIO_InitTypeDef GPIO_InitStruct = {0};
    
      /* GPIO Ports Clock Enable */
      __HAL_RCC_GPIOC_CLK_ENABLE();
      __HAL_RCC_GPIOD_CLK_ENABLE();
      __HAL_RCC_GPIOA_CLK_ENABLE();
      __HAL_RCC_GPIOB_CLK_ENABLE();
    
      /*Configure GPIO pin Output Level */
      HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10, GPIO_PIN_RESET);
    
      /*Configure GPIO pin : B1_Pin */
      GPIO_InitStruct.Pin = B1_Pin;
      GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
    
      /*Configure GPIO pins : LD2_Pin PA8 PA9 PA10 */
      GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
      GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
      HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
      /* EXTI interrupt init*/
      HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
      HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
    
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
      * @brief  This function is executed in case of error occurrence.
      * @retval None
      */
    void Error_Handler(void)
    {
      /* USER CODE BEGIN Error_Handler_Debug */
      /* User can add his own implementation to report the HAL error return state */
    
      /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef  USE_FULL_ASSERT
    /**
      * @brief  Reports the name of the source file and the source line number
      *         where the assert_param error has occurred.
      * @param  file: pointer to the source file name
      * @param  line: assert_param error line source number
      * @retval None
      */
    void assert_failed(uint8_t *file, uint32_t line)
    {
      /* USER CODE BEGIN 6 */
      /* User can add his own implementation to report the file name and line number,
         tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
      /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    
    /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
    
    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2021, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    
    //******************************************************************************
    //   BQ76952EVM demo code for MSP430FR2x55 + BQ769x2
    //
    //   Description: MSP430FR2x55 functions as the I2C host that communicates
    //   with the BQ769x2 sending and receiving different types of commands. 
    //   ACLK = 32.768kHz REFO or external XT1, MCLK = SMCLK = ~16MHz DCO
    //
    //                                     /|\ /|\
    //                    MSP430FR2x55     10k  |
    //                 -----------------    |  10k
    //            /|\ |             P4.6|---+---|-- I2C Data (UCB1SDA)
    //             |  |                 |       |
    //             ---|RST          P4.7|-------+-- I2C Clock (UCB1SCL)
    //                |                 |
    //                |             P2.3|---> SHUT
    //                |                 |
    //                |             P4.2|---> FETOFF
    //                |                 |
    //       LED1 <---|P1.1         P4.3|<--- ALERT
    //                |                 |
    //
    //
    //   Andrew Han and Matt Sunna
    //   Texas Instruments Inc.
    //   August 2021
    //   Built with Code Composer Studio (CCS) v10.1.1
    //******************************************************************************
    
    // Includes
    #include <msp430.h>
    #include <stdio.h>
    #include <stdint.h>
    #include <stdbool.h>
    #include <Include/HAL.h>
    #include <Include/QmathLib.h>
    #include <Include/callbacks_mpack.h>
    #include "BQ769x2Header.h"
    
    // Defines
    #define DEV_ADDR  0x08  // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address
    #define CRC_Mode 0  // 0 for disabled, 1 for enabled
    #define MAX_BUFFER_SIZE         10
    #define R 0 //Read
    #define W 1 //Write
    #define W2 2 //write data with two bytes
    
    
    // Arrays
    uint8_t RX_data [2] = {0x00, 0x00};// used for DirectCommand func, 
    uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 
    	0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    
    
    
    //******************************************************************************
    // I2C State Machine ***********************************************************
    //******************************************************************************
    
    typedef enum I2C_ModeEnum{
        IDLE_MODE,
        NACK_MODE,
        TX_REG_ADDRESS_MODE,
        RX_REG_ADDRESS_MODE,
        TX_DATA_MODE,
        RX_DATA_MODE,
        SWITCH_TO_RX_MODE,
        SWITHC_TO_TX_MODE,
        TIMEOUT_MODE
    } I2C_Mode;
    
    /* Used to track the state of the software state machine*/
    I2C_Mode MasterMode = IDLE_MODE;
    
    /* Register address/command to use*/
    uint8_t TransmitRegAddr = 0;
    
    /* ReceiveBuffer: Buffer used to receive data in the ISR
     * RXByteCtr: Number of bytes left to receive
     * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
     * TransmitBuffer: Buffer used to transmit data in the ISR
     * TXByteCtr: Number of bytes left to transfer
     * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
     */
    uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t RXByteCtr = 0;
    uint8_t ReceiveIndex = 0;
    uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
    uint8_t TXByteCtr = 0;
    uint8_t TransmitIndex = 0;
    
    //******************************************************************************
    // BQ Parameters ***************************************************************
    //******************************************************************************
    
    // Global Variables for cell voltages, temperatures, Stack voltage, PACK Pin voltage, LD Pin voltage, CC2 current
    uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    float Temperature [3] = {0,0,0};
    uint16_t Stack_Voltage = 0x00;
    uint16_t Pack_Voltage = 0x00;
    uint16_t LD_Voltage = 0x00;
    uint16_t Pack_Current = 0x00;
    uint16_t AlarmBits = 0x00;
    
    uint8_t value_SafetyStatusA;  // Safety Status Register A
    uint8_t value_SafetyStatusB;  // Safety Status Register B
    uint8_t value_SafetyStatusC;  // Safety Status Register C
    uint8_t value_PFStatusA;   // Permanent Fail Status Register A
    uint8_t value_PFStatusB;   // Permanent Fail Status Register B
    uint8_t value_PFStatusC;   // Permanent Fail Status Register C
    uint8_t FET_Status;  // FET Status register contents  - Shows states of FETs
    uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
    
    uint8_t	UV_Fault = 0;   // under-voltage fault state
    uint8_t	OV_Fault = 0;   // over-voltage fault state
    uint8_t	SCD_Fault = 0;  // short-circuit fault state
    uint8_t	OCD_Fault = 0;  // over-current fault state
    uint8_t ProtectionsTriggered = 0; // Set to 1 if any protection triggers
    
    uint8_t LD_ON = 0;							// Load Detect status bit
    uint8_t DSG = 0;   // discharge FET state
    uint8_t CHG = 0;   // charge FET state
    uint8_t PCHG = 0;  // pre-charge FET state
    uint8_t PDSG = 0;  // pre-discharge FET state
    
    uint32_t AccumulatedCharge_Int; // in AFE_READPASSQ func
    uint32_t AccumulatedCharge_Frac;// in AFE_READPASSQ func
    uint32_t AccumulatedCharge_Time;// in AFE_READPASSQ func
    
    
    //******************************************************************************
    // Function prototypes *********************************************************
    //******************************************************************************
    
    void GPIO_initPins(void);
    void GPIO_configPins(void);
    void UCS_initModule(void);
    void I2C_initModule(void);
    void UART_initPins(void);
    void Software_Trim(void);
    
    void delayUS(uint16_t us) {   // Sets the delay in microseconds.
        uint16_t ms;
        char i;
        ms = us / 1000;
        for(i=0; i< ms; i++)
            __delay_cycles(16000);
    }
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    unsigned char Checksum(unsigned char *ptr, unsigned char len)	
    {
        // Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
    	unsigned char i;
    	unsigned char checksum = 0;
    
    	for(i=0; i<len; i++)
    		checksum += ptr[i];
    
    	checksum = 0xff & ~checksum;
    
    	return(checksum);
    }
    
    unsigned char CRC8(unsigned char *ptr, unsigned char len)
    {
    	unsigned char i;
    	unsigned char crc=0;
    	while(len--!=0)
    	{
    		for(i=0x80; i!=0; i/=2)
    		{
    			if((crc & 0x80) != 0)
    			{
    				crc *= 2;
    				crc ^= 0x107;
    			}
    			else
    				crc *= 2;
    
    			if((*ptr & i)!=0)
    				crc ^= 0x107;
    		}
    		ptr++;
    	}
    	return(crc);
    }
    
    I2C_Mode I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
        /* Initialize state machine */
        MasterMode = TX_REG_ADDRESS_MODE;
        TransmitRegAddr = reg_addr;
        RXByteCtr = count;
        TXByteCtr = 0;
        ReceiveIndex = 0;
        TransmitIndex = 0;
    
        /* Initialize device address and interrupts */
        UCB1I2CSA = DEV_ADDR;
        UCB1IFG &= ~(UCTXIFG + UCRXIFG);        // Clear any pending interrupts
        UCB1IE &= ~UCRXIE;                      // Disable RX interrupt
        UCB1IE |= UCTXIE;                       // Enable TX interrupt
        UCB1CTLW0 |= UCTR + UCTXSTT;            // I2C TX, start condition
        __bis_SR_register(LPM0_bits + GIE);     // Enter LPM0 w/ interrupts
        //For debugger
        __no_operation();
    
        /* Copy over received data */
        CopyArray(ReceiveBuffer, reg_data, count);
    
        return MasterMode;
    }
    
    I2C_Mode I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
        /* Initialize state machine */
        MasterMode = TX_REG_ADDRESS_MODE;
        TransmitRegAddr = reg_addr;
    
        /* Copy register data to TransmitBuffer */
        CopyArray(reg_data, TransmitBuffer, count);
    
        TXByteCtr = count;
        RXByteCtr = 0;
        ReceiveIndex = 0;
        TransmitIndex = 0;
    
        /* Initialize device address and interrupts */
        UCB1I2CSA = DEV_ADDR;
        UCB1IFG &= ~(UCTXIFG + UCRXIFG);        // Clear any pending interrupts
        UCB1IE &= ~UCRXIE;                      // Disable RX interrupt
        UCB1IE |= UCTXIE;                       // Enable TX interrupt
        UCB1CTLW0 |= UCTR + UCTXSTT;            // I2C TX, start condition
        __bis_SR_register(LPM0_bits + GIE);     // Enter LPM0 w/ interrupts
        //For debugger
        __no_operation();
    
        return MasterMode;
    }
    
    void AFE_SetRegister(uint16_t reg_addr, uint32_t reg_data, uint8_t datalen)
    {
    	//reg_data needs to be in the correct format (little endian)
      uint8_t TX_RegData2[2] = {0x00, 0x00};
      uint8_t TX_RegData3[3] = {0x00, 0x00, 0x00};
      uint8_t TX_RegData4[4] = {0x00, 0x00, 0x00, 0x00};
      uint8_t TX_RegData6[6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    	switch(datalen)
        {
    		case 1:
    			TX_RegData3[0] = reg_addr & 0xff;
    			TX_RegData3[1] = (reg_addr >> 8) & 0xff;
    			TX_RegData3[2] = reg_data & 0xff;
          		I2C_WriteReg(0x3E, TX_RegData3, 3);
    			delayUS(2000);
    			TX_RegData2[0] = Checksum(TX_RegData3, 3); TX_RegData2[1] = 0x05;  // Checksum and Length
          		I2C_WriteReg(0x60, TX_RegData2, 2);
    			delayUS(2000);
    			break;
    		case 2:
    			TX_RegData4[0] = reg_addr & 0xff;
    			TX_RegData4[1] = (reg_addr >> 8) & 0xff;
    			TX_RegData4[2] = reg_data & 0xff;
    			TX_RegData4[3] = (reg_data >> 8) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData4, 4);
    			delayUS(2000);
    			TX_RegData2[0] = Checksum(TX_RegData4, 4); TX_RegData2[1] = 0x06;  // Checksum and Length
          		I2C_WriteReg(0x60, TX_RegData2, 2);
    			delayUS(2000);
    			break;
    		case 4: //Only used for CCGain and Capacity Gain
    			TX_RegData6[0] = reg_addr & 0xff;
    			TX_RegData6[1] = (reg_addr >> 8) & 0xff;
    			TX_RegData6[2] = reg_data & 0xff;
    			TX_RegData6[3] = (reg_data >> 8) & 0xff;
    			TX_RegData6[4] = (reg_data >> 16) & 0xff;
    			TX_RegData6[5] = (reg_data >> 24) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData6, 6);
    			delayUS(2000);
    			TX_RegData2[0] = Checksum(TX_RegData6, 6); TX_RegData2[1] = 0x08;  // Checksum and Length
          		I2C_WriteReg(0x60, TX_RegData2, 2);
    			delayUS(2000);
    			break;
        }
    }
    
    void CommandSubcommands(uint16_t command) //For Command only Subcommands
    {	//For DEEPSLEEP subcommand need to call this function twice
    	//Make sure to place delay after this function is called
    	uint8_t TX_Reg[2] = {0x00, 0x00};
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff;
    	I2C_WriteReg(0x3E,TX_Reg,2); 
    }
    
    void Subcommands(uint16_t command, uint16_t data, uint8_t type)
    {
    	//security keys and Manu_data writes dont work with this function (reading these commands works)
    	//max readback size is 32 bytes i.e. DASTATUS, CUV/COV snapshot
    	uint8_t TX_Reg2[2] = {0x00, 0x00};
    	uint8_t TX_Reg3[3] = {0x00, 0x00, 0x00};
    	uint8_t TX_Reg4[4] = {0x00, 0x00, 0x00, 0x00};
    
    	if (type == R) {//read
    		TX_Reg2[0] = command & 0xff;
    		TX_Reg2[1] = (command >> 8) & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg2,2);
    		delayUS(2000);
    		I2C_ReadReg(0x40, RX_32Byte, 32); 
    	}
    	if (type == W) {
    		//FET_Control, REG12_Control
    		TX_Reg3[0] = command & 0xff;
    		TX_Reg3[1] = (command >> 8) & 0xff;
    		TX_Reg3[2] = data & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg3,3);
    		delayUS(2000);
    		TX_Reg2[0] = Checksum(TX_Reg3, 3); TX_Reg2[1] = 0x05;
    		I2C_ReadReg(0x60, TX_Reg2, 2); 
    	}
    	if (type == W2){ //write data with 2 bytes
    		//CB_Active_Cells, CB_SET_LVL
    		TX_Reg4[0] = command & 0xff;
    		TX_Reg4[1] = (command >> 8) & 0xff;
    		TX_Reg4[2] = data & 0xff;
    		TX_Reg4[3] = (data >> 8) & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg4,4);
    		delayUS(2000);
    		TX_Reg2[0] = Checksum(TX_Reg4, 4); TX_Reg2[1] = 0x05;
    		I2C_ReadReg(0x60, TX_Reg2, 2); 
    	}
    }
    
    void DirectCommand(uint8_t command, uint16_t data, uint8_t type)
    {	//type: R = read, W = write
        //RX_data global var
    	uint8_t TX_data[2] = {0x00, 0x00};
    	TX_data[0] = data & 0xff;
    	TX_data[1] = (data >> 8) & 0xff;
    	if (type == R) {//Read
    		I2C_ReadReg(command, RX_data, 2); 
    	}
    	if (type == W) {//write
        //Control_status, alarm_status, alarm_enable all 2 bytes long
    		I2C_WriteReg(command,TX_data,2);
    	}
    }
    
    void AFE_Init() {
    	// Configures all parameters in device RAM
    
    	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
    	// See TRM for full description of CONFIG_UPDATE mode
    	CommandSubcommands(SET_CFGUPDATE);
    
    	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
    	// programmed for the change to take effect. All of the RAM registers are described in detail in Chapter 13 of the BQ76952 TRM.
    	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
    	// a full description of the register and the bits will pop up on the screen.
    	// A summary of the Data Memory is also in Section 13.9 of the TRM.
    
    	// 'Power Config' - Set DSLP_LDO  - 0x9234 = 0x2D80
    	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
      // Set wake speed bits to 00 for best performance
    	AFE_SetRegister(PowerConfig, 0x2D80, 2);
    
    	// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
    	AFE_SetRegister(REG0Config, 0x01, 1);
    
    	// 'REG12 Config' - Enable REG1 with 3.3V output (0x0D for 3.3V, 0x0F for 5V)
    	AFE_SetRegister(REG12Config, 0x0D, 1);
    
    	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000, 0x0000 is default value
    	AFE_SetRegister(VCellMode, 0x0000, 2);
    
    	// 'Default Alarm Mask' - Enable FullScan and ADScan bits
    	// 0xF882
    	AFE_SetRegister(DefaultAlarmMask, 0xF882, 2);
    
    	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC
    	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
    	// COV (over-voltage), CUV (under-voltage)
    	AFE_SetRegister(EnabledProtectionsA, 0xBC, 1);
    
    	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7
    	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
    	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
    	AFE_SetRegister(EnabledProtectionsB, 0xF7, 1);
    
    	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07
    	AFE_SetRegister(TS1Config, 0x07, 1);
    
    	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F
    	AFE_SetRegister(TS3Config, 0x0F, 1);
    
    	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
    	AFE_SetRegister(DFETOFFPinConfig, 0x42, 1);
    
    	// Set up Alert Pin - 0x92FC = 0x2A
    	// This configures the Alert pin to drive high (REG1 voltage) when enabled.
    	// Other options available include active-low, drive HiZ, drive using REG18 (1.8V), weak internal pull-up and pull-down
    	AFE_SetRegister(ALERTPinConfig, 0x2A, 1);
    
    	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
    	// Chapter 10 of TRM describes Cell Balancing in detail
    	// Also see "Cell Balancing with BQ76952, BQ76942 Battery Monitors" document on ti.com
    	AFE_SetRegister(BalancingConfiguration, 0x03, 1);
    
    	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
    	// COV Threshold is this value multiplied by 50.6mV
    	AFE_SetRegister(COVThreshold, 0x55, 1);
    
    	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)
    	// 0x05=100mV
    	AFE_SetRegister(SCDThreshold, 0x05, 1);
    
    	// Set up SCD Delay - 0x9287 = 0x03 (30 us)    
    	// Units of 15us
    	AFE_SetRegister(SCDDelay, 0x03, 1);
    
    	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
    	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
    	AFE_SetRegister(SCDLLatchLimit, 0x01, 1);
    
    	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
    	CommandSubcommands(EXIT_CFGUPDATE);
    }
    
    //  ********************************* FET Control Commands  ***************************************
    
    void AFE_BOTHOFF () {
    	// Disables all FETs using the DFETOFF (BOTHOFF) pin
    	P4OUT |= BIT2;              // Set DFETOFF pin
    }
    
    void AFE_RESET_BOTHOFF () {
    	// Resets DFETOFF (BOTHOFF) pin
    	P4OUT &= ~BIT2;             // Reset DFETOFF pin
    }
    
    void AFE_ReadFETStatus() { 
    	// Read FET Status to see which FETs are enabled
    	DirectCommand(FETStatus, 0x00, R);
    	FET_Status = (RX_data[1]*256 + RX_data[0]);
    	DSG = ((0x4 & RX_data[0])>>2);// discharge FET state
      	CHG = (0x1 & RX_data[0]);// charge FET state
      	PCHG = ((0x2 & RX_data[0])>>1);// pre-charge FET state
      	PDSG = ((0x8 & RX_data[0])>>3);// pre-discharge FET state
    }
    
    // ********************************* End of FET Control Commands *********************************
    
    // ********************************* AFE Power Commands   *****************************************
    
    void AFE_ShutdownPin() {
    	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
    	P2OUT |= BIT3;              // Set DFETOFF pin
    }
    
    void AFE_ReleaseShutdownPin() {
    	// Releases the RST_SHUT pin
    	P2OUT &= ~BIT3;             // Reset DFETOFF pin
    }
    
    // ********************************* End of AFE Power Commands   *****************************************
    
    
    // ********************************* AFE Status and Fault Commands   *****************************************
    
    uint16_t AFE_ReadAlarmStatus() { 
    	// Read this register to find out why the Alert pin was asserted. 
    	DirectCommand(AlarmStatus, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);
    }
    
    void AFE_ReadSafetyStatus() { //good example functions
    	// Read Safety Status A/B/C and find which bits are set
    	// This shows which primary protections have been triggered
    	DirectCommand(SafetyStatusA, 0x00, R);
    	value_SafetyStatusA = (RX_data[1]*256 + RX_data[0]);
    	//Example Fault Flags
    	UV_Fault = ((0x4 & RX_data[0])>>2);
    	OV_Fault = ((0x8 & RX_data[0])>>3);
    	SCD_Fault = ((0x8 & RX_data[1])>>3);
    	OCD_Fault = ((0x2 & RX_data[1])>>1);
    	DirectCommand(SafetyStatusB, 0x00, R);
    	value_SafetyStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommand(SafetyStatusC, 0x00, R);
    	value_SafetyStatusC = (RX_data[1]*256 + RX_data[0]);
    	if ((value_SafetyStatusA + value_SafetyStatusB + value_SafetyStatusC) > 1) {
    		ProtectionsTriggered = 1; }
    	else {
    		ProtectionsTriggered = 0; }
    }
    
    void AFE_ReadPFStatus() {
    	// Read Permanent Fail Status A/B/C and find which bits are set
    	// This shows which permanent failures have been triggered
    	DirectCommand(PFStatusA, 0x00, R);
    	value_PFStatusA = (RX_data[1]*256 + RX_data[0]);
    	DirectCommand(PFStatusB, 0x00, R);
    	value_PFStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommand(PFStatusC, 0x00, R);
    	value_PFStatusC = (RX_data[1]*256 + RX_data[0]);
    }
    
    // ********************************* End of AFE Status and Fault Commands   *****************************************
    
    
    // ********************************* AFE Measurement Commands   *****************************************
    
    
    uint16_t AFE_ReadVoltage(uint8_t command)
    {
    	//RX_data is global var
    	DirectCommand(command, 0x00, R);
    	if(command >= Cell1Voltage && command <= Cell16Voltage) {//Cells 1 through 16 (0x14 to 0x32)
    		return (RX_data[1]*256 + RX_data[0]); //voltage is reported in mV
    	}
    	else {//stack, Pack, LD
    		return 10 * (RX_data[1]*256 + RX_data[0]); //voltage is reported in 0.01V units
    	}
    
    }
    
    void AFE_ReadAllVoltages()
    {
      int cellvoltageholder = Cell1Voltage;
      int x;
      for (x = 0; x < 16; x++){         //Reads all cell voltages
        CellVoltage[x] = AFE_ReadVoltage(cellvoltageholder);
        cellvoltageholder = cellvoltageholder + 2;
      }
      Stack_Voltage = AFE_ReadVoltage(StackVoltage);
      Pack_Voltage = AFE_ReadVoltage(PACKPinVoltage);
      LD_Voltage = AFE_ReadVoltage(LDPinVoltage);
    }
    
    uint16_t AFE_ReadCurrent() {
    	DirectCommand(CC2Current, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);  // current is reported in mA
    }
    
    float AFE_ReadTemperature(uint8_t command) {
    	//RX_data is a global var
    	switch(command)
    	{
    		case TS1Temperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case TS3Temperature:
    			DirectCommand(command, 0x00, R); 
    			break;
    		case HDQTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case DCHGTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case DDSGTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case CFETOFFTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case DFETOFFTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case ALERTTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case IntTemperature:
    			DirectCommand(command, 0x00, R);
    			break;
    		case TS2Temperature:
    			DirectCommand(command, 0x00, R); //Not advised to use TS2 as a temp sensor if Shutdown is used 
                break;
    		default: break;
    	}
    	return (0.1 * (float)(RX_data[1]*256 + RX_data[0])) - 273.15;  // convert from 0.1K to Celcius
    }
    
                            //*********************************NEED TO DEBUG THIS FOR 32BYTE Array
    
    void AFE_ReadPassQ(){ // Read Accumulated Charge and Time from DASTATUS6 
    	Subcommands(DASTATUS6, 0x00, R);
    	AccumulatedCharge_Int = ((RX_32Byte[3]<<24) + (RX_32Byte[2]<<16) + (RX_32Byte[1]<<8) + RX_32Byte[0]);
    	AccumulatedCharge_Frac = ((RX_32Byte[7]<<24) + (RX_32Byte[6]<<16) + (RX_32Byte[5]<<8) + RX_32Byte[4]);
    	AccumulatedCharge_Time = ((RX_32Byte[11]<<24) + (RX_32Byte[10]<<16) + (RX_32Byte[9]<<8) + RX_32Byte[8]);
    }
    
    
    //******************************************************************************
    // main ************************************************************************
    //******************************************************************************
    int main(void)
    {
        // Stop watchdog timer
        WDTCTL = WDTPW | WDTHOLD;
    	
        // Initialize GPIOs, clocks and peripherals
        GPIO_initPins();
        UCS_initModule();
        I2C_initModule();
    
    	CommandSubcommands(RESET); //AFE_Reset();
    	delayUS(60000);
    	AFE_Init();
    	delayUS(10000);
    	CommandSubcommands(FET_ENABLE); //AFE_FET_ENABLE();
    	delayUS(10000);
    	CommandSubcommands(SLEEP_DISABLE); //AFE_SLEEP_DISABLE();
    
    	delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000);  //wait to start measurements after FETs close
    
    
        // Infinite loop
        while(1)
        {
    		AlarmBits = AFE_ReadAlarmStatus();
    		if (AlarmBits & 0x80) {  // Check if FULLSCAN is complete. If set, new measurements are available
          		AFE_ReadAllVoltages();
          		Pack_Current = AFE_ReadCurrent();
          		Temperature[0] = AFE_ReadTemperature(TS1Temperature);
          		Temperature[1] = AFE_ReadTemperature(TS3Temperature);
    			DirectCommand(AlarmStatus, 0x0080, W);  // Clear FULLSCAN bit
    		}
    				
    		if (AlarmBits & 0xC000) {  // If Safety Status bits are showing in AlarmStatus register
    			AFE_ReadSafetyStatus();
    			if (ProtectionsTriggered & 1) {
    				P1OUT |= BIT0;             } // Turn on LED to indicate protection triggered
    				DirectCommand(AlarmStatus, 0xF800, W); // Clear the Safety Status Alarm bits
    			}
    		else
    		{
    			if (ProtectionsTriggered & 1) {
    				AFE_ReadSafetyStatus();
    				if (!(ProtectionsTriggered & 1)) {
    					P1OUT &= ~BIT0; }   // Turn off LED if Safety has cleared
    			} // Turn off the LED if Safety Status has cleared
    		}
    		delayUS(20000);  // repeat loop every 20 ms
    	}
    }
    
    
    void GPIO_initPins()
    {
        // Initialize all pins to output low, except P4.5
        P1OUT = 0x00; P2OUT = 0x00;
        P3OUT = 0x00; P4OUT = 0x00;
        P5OUT = 0x00; P6OUT = 0x00;
    
        P1DIR = 0xFF; P2DIR = 0xFF;
        P3DIR = 0xFF; P4DIR = 0xFF;
        P5DIR = 0xFF; P6DIR = 0xFF;
    
        // Configure GPIOs
        GPIO_configPins();
    
        // Disable the GPIO power-on default high-impedance mode to activate
        // previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    }
    
    void GPIO_configPins()
    {
        /* Inputs */
    
        // Button S1
        P4DIR &= ~BIT1;                 // Set P4.1 as input
        P4REN |= BIT1;                  // Enable internal resistor
        P4OUT |= BIT1;                  // Set pull-up on this pin
    
        // Button S2
        P2DIR &= ~BIT3;                 // Set P2.3 as input
        P2REN |= BIT3;                  // Enable internal resistor
        P2OUT |= BIT3;                  // Set pull-up on this pin
    
        /* Outputs */
    
        // P1.0 (LED1)
        P1OUT &= ~BIT0;                 // Set P1.0 to low
        P1DIR |= BIT0;                  // Set P1.0 to output direction
    
        // P6.6 (LED2)
        P6OUT &= ~BIT6;                 // Set P6.6 to low
        P6DIR |= BIT6;                  // Set P6.6 to output direction
    
    }
    
    void UCS_initModule()
    {
    #ifdef __ENABLE_XT1__
        // Configure XT1 pins
        P2SEL0 |= BIT6 | BIT7;
        do
        {
            CSCTL7 &= ~(XT1OFFG | DCOFFG);     // Clear XT1 and DCO fault flags
            SFRIFG1 &= ~OFIFG;
        }while (SFRIFG1 & OFIFG);              // Test oscillator fault flag
    #endif
    
        // Configure one FRAM waitstate as required by the device datasheet for MCLK
        // operation beyond 8MHz _before_ configuring the clock system.
        FRCTL0 = FRCTLPW | NWAITS_1;
    
        // Clock System Setup
        __bis_SR_register(SCG0);                           // Disable FLL
    #ifdef __ENABLE_XT1__
        CSCTL3 |= SELREF__XT1CLK;                          // Set XT1 as FLL reference source
    #else
        CSCTL3 |= SELREF__REFOCLK;                         // Set REFO as FLL reference source
    #endif
        CSCTL0 = 0;                                        // clear DCO and MOD registers
        CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
        CSCTL1 |= DCORSEL_5;                               // Set DCO = 16MHz
        CSCTL2 = FLLD_0 + 487;                             // DCOCLKDIV = 16MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                           // Enable FLL
        Software_Trim();                                   // Software Trim to get the best DCOFTRIM value
    #ifdef __ENABLE_XT1__
        CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK;          // MCLK = SMCLK = DCO; ACLK = XT1 (external)
    #else
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;         // MCLK = SMCLK = DCO; ACLK = REFO (internal)
    #endif
    }
    
    void I2C_initModule()
    {
        // Configure I2C pins
        P4SEL0 |= BIT6 | BIT7;
        P4SEL1 &= ~(BIT6 | BIT7);
    
        // Configure I2C peripheral
        UCB1CTLW0 = UCSWRST;                                    // Enable SW reset
        UCB1CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C host mode, SMCLK
        UCB1BRW = 40;                                           // fSCL = SMCLK/40 = ~400kHz
        UCB1I2CSA = DEV_ADDR;                            // Device Address
        UCB1CTLW0 &= ~UCSWRST;                                  // Clear SW reset, resume operation
        UCB1IE |= UCNACKIE;
    }
    
    void UART_initPins()
    {
        // Configure UART pins, module is configured in HAL_GUIComm_UART_FR235x.c
        P4SEL0 |= BIT2 | BIT3;
        P4SEL1 &= ~(BIT2 | BIT3);
    }
    
    
    void Software_Trim()
    {
        unsigned int oldDcoTap = 0xffff;
        unsigned int newDcoTap = 0xffff;
        unsigned int newDcoDelta = 0xffff;
        unsigned int bestDcoDelta = 0xffff;
        unsigned int csCtl0Copy = 0;
        unsigned int csCtl1Copy = 0;
        unsigned int csCtl0Read = 0;
        unsigned int csCtl1Read = 0;
        unsigned int dcoFreqTrim = 3;
        unsigned char endLoop = 0;
    
        do
        {
            CSCTL0 = 0x100;                         // DCO Tap = 256
            do
            {
                CSCTL7 &= ~DCOFFG;                  // Clear DCO fault flag
            }while (CSCTL7 & DCOFFG);               // Test DCO fault flag
    
            __delay_cycles((unsigned int)3000 * CPU_FREQ_MHZ);  // Wait FLL lock status (FLLUNLOCK) to be stable
                                                                // Suggest to wait 24 cycles of divided FLL reference clock
            while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0));
    
            csCtl0Read = CSCTL0;                   // Read CSCTL0
            csCtl1Read = CSCTL1;                   // Read CSCTL1
    
            oldDcoTap = newDcoTap;                 // Record DCOTAP value of last time
            newDcoTap = csCtl0Read & 0x01ff;       // Get DCOTAP value of this time
            dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value
    
            if(newDcoTap < 256)                    // DCOTAP < 256
            {
                newDcoDelta = 256 - newDcoTap;     // Delta value between DCPTAP and 256
                if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256
                    endLoop = 1;                   // Stop while loop
                else
                {
                    dcoFreqTrim--;
                    CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
                }
            }
            else                                   // DCOTAP >= 256
            {
                newDcoDelta = newDcoTap - 256;     // Delta value between DCPTAP and 256
                if(oldDcoTap < 256)                // DCOTAP cross 256
                    endLoop = 1;                   // Stop while loop
                else
                {
                    dcoFreqTrim++;
                    CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
                }
            }
    
            if(newDcoDelta < bestDcoDelta)         // Record DCOTAP closest to 256
            {
                csCtl0Copy = csCtl0Read;
                csCtl1Copy = csCtl1Read;
                bestDcoDelta = newDcoDelta;
            }
    
        }while(endLoop == 0);                      // Poll until endLoop == 1
    
        CSCTL0 = csCtl0Copy;                       // Reload locked DCOTAP
        CSCTL1 = csCtl1Copy;                       // Reload locked DCOFTRIM
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
    }
    
    //******************************************************************************
    // I2C Interrupt ***************************************************************
    //******************************************************************************
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = USCI_B1_VECTOR
    __interrupt void USCI_B1_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCI_B1_VECTOR))) USCI_B1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      // Must read from UCB1RXBUF
      uint8_t rx_val = 0;
      switch(__even_in_range(UCB1IV, USCI_I2C_UCBIT9IFG))
      {
        case USCI_NONE:          break;         // Vector 0: No interrupts
        case USCI_I2C_UCALIFG:   break;         // Vector 2: ALIFG
        case USCI_I2C_UCNACKIFG:                // Vector 4: NACKIFG
          break;
        case USCI_I2C_UCSTTIFG:  break;         // Vector 6: STTIFG
        case USCI_I2C_UCSTPIFG:  break;         // Vector 8: STPIFG
        case USCI_I2C_UCRXIFG3:  break;         // Vector 10: RXIFG3
        case USCI_I2C_UCTXIFG3:  break;         // Vector 12: TXIFG3
        case USCI_I2C_UCRXIFG2:  break;         // Vector 14: RXIFG2
        case USCI_I2C_UCTXIFG2:  break;         // Vector 16: TXIFG2
        case USCI_I2C_UCRXIFG1:  break;         // Vector 18: RXIFG1
        case USCI_I2C_UCTXIFG1:  break;         // Vector 20: TXIFG1
        case USCI_I2C_UCRXIFG0:                 // Vector 22: RXIFG0
            rx_val = UCB1RXBUF;
            if (RXByteCtr)
            {
              ReceiveBuffer[ReceiveIndex++] = rx_val;
              RXByteCtr--;
            }
    
            if (RXByteCtr == 1)
            {
              UCB1CTLW0 |= UCTXSTP;
            }
            else if (RXByteCtr == 0)
            {
              UCB1IE &= ~UCRXIE;
              MasterMode = IDLE_MODE;
              __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
            }
            break;
        case USCI_I2C_UCTXIFG0:                 // Vector 24: TXIFG0
            switch (MasterMode)
            {
              case TX_REG_ADDRESS_MODE:
                  UCB1TXBUF = TransmitRegAddr;
                  if (RXByteCtr)
                      MasterMode = SWITCH_TO_RX_MODE;   // Need to start receiving now
                  else
                      MasterMode = TX_DATA_MODE;        // Continue to transmission with the data in Transmit Buffer
                  break;
    
              case SWITCH_TO_RX_MODE:
                  UCB1IE |= UCRXIE;                     // Enable RX interrupt
                  UCB1IE &= ~UCTXIE;                    // Disable TX interrupt
                  UCB1CTLW0 &= ~UCTR;                   // Switch to receiver
                  MasterMode = RX_DATA_MODE;            // State state is to receive data
                  UCB1CTLW0 |= UCTXSTT;                 // Send repeated start
                  if (RXByteCtr == 1)
                  {
                      // Must send stop since this is the N-1 byte
                      while((UCB1CTLW0 & UCTXSTT));
                      UCB1CTLW0 |= UCTXSTP;             // Send stop condition
                  }
                  break;
    
              case TX_DATA_MODE:
                  if (TXByteCtr)
                  {
                      UCB1TXBUF = TransmitBuffer[TransmitIndex++];
                      TXByteCtr--;
                  }
                  else
                  {
                      // Done with transmission
                      UCB1CTLW0 |= UCTXSTP;                 // Send stop condition
                      MasterMode = IDLE_MODE;
                      UCB1IE &= ~UCTXIE;                    // Disable TX interrupt
                      __bic_SR_register_on_exit(CPUOFF);    // Exit LPM0
                  }
                  break;
    
              default:
                  __no_operation();
                  break;
            }
            break;
        default: break;
      }
    }
    

    Best regards,

    Matt