This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010: 36Vout/10mA boost converter

Part Number: LMR64010
Other Parts Discussed in Thread: LM5157, , TPS55340

Hi Team,

I'm looking for boost converter supporting following requirement.

LMR64010, TPS55340 and LM5157 would be one of candidates but which one is recommended boost converter for below requirement?

I checked duty cycle and minimum on time but if there are any other parameter that I have to care about, please let me know.

[Requirement]

Vin: 10V or 24V

Vout: 36V

Iout: ~10mA

fsw: higher switching frequency to isolate analog.

Duty=1-Vin/(Vout+Vf)=34%(24Vin), 73%(10Vin) ※Vf=0.5V

LMR64010: 73%(10Vin) < 87% max duty cycle

TPS55340: 34%(24Vin), 73%(10Vin) < 89% max duty cycle

LM5157: 34%(24Vin), 73%(10Vin) < 80% max duty cycle(RT=90.9k)

Regards,

Kai