This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: Clock synchronisation range

Part Number: TPS55288


Hi all,

I would like to use the clock synchronisation on the TPS55288 however it only works in a very small range.

FSW is connected to ground via 68k resistor. Without synchronisation the measured frequency is ~289kHz. The clock is generated with an waveform generator (4Vpp, 2V Offset, square wave) and connected to the DITH/SYNC pin. The capacitor for frequency dithering is removed. The switching frequency gets synchronised between 281kHz and 291kHz, above or below the synchronisation gets lost and the TPS switches with 289kHz again. However the datasheet specifies the pulling range with +-30%.

Have tried it with 3 different boards and got the same result.

Best regards,

Michael