Is it possible for the current limiting function to operate in response to the inrush current?
If so, what kind of load can prevent the current limiting function from working?
Is it possible to specify by the input capacity of the load?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible for the current limiting function to operate in response to the inrush current?
If so, what kind of load can prevent the current limiting function from working?
Is it possible to specify by the input capacity of the load?
Hi Takayuki,
LM2594 is with peak current limit feature and the typical current limit value is 0.8A. You can calculate the inrush current giving the condition of output voltage and capacitance to see it it will trigger the peak current limit.
If it is so, you can also consider the delayed start-up function in datasheet section 8.3.1, where the input capacitor is allowed to charge up to a higher voltage
before the switcher begins operating. A portion of the high input current needed for start-up is now supplied by the input capacitor .
Regards,
Xiaoying
Hi Takayuki,
If you have no more questions, pls help click "resolved" button for us to close this thread.
BR
Xiaoying
What are the conditions under which current limiting works?
Isn't there a lower limit of the current threshold and a duration condition?
Hi Takayuki,
The current limit is fixed and you can find the typical value, min value and max value in the datasheet (temperature variation will influence the sense and limit results).
But we don't have any mechanism to change the current limit under a duration condition.
Regards,
Xiaoying
Hi Takayuki,
If you have no more questions, pls help click "resolved" button for us to close this thread.
BR
Xiaoying