Hi team ,
I have test the hiccup protection mode of TPS56C15. I have some confusion which might needs your help and support .
1. About over current protection
As is shown in the datasheet ,"the UVP comparator detects it and shuts down the device after a wait time of 1 ms , the device restarts after a hiccup time of 7 ms . " From my perspective , when over current happens , the vout is pulled down until to 0.68 vout_normal , after which the hiccup mode is triggered .Basically speaking , the over current protection finally triggers the under voltage protect , doesn't it ?
2 . Waiting time
I have read the Meng Liu's e2e question , though there are still some more confusion . Firstly , the waiting time is still 1ms according to my test (where current is 13A and Vout is drained down to 0.8V, first protection ). After a gap of 18ms , restart is triggered . And the voltage ramps up to 1V , which takes about 1 ms (not 4.7ms ?) I'm confused why not 4.7 ms ? Also thw waiting time when Iout stays at 13A and vout at 0.8V is longer than first protection . Is that because the converter is still on the soft start mode , in which case the device can tolerate longer under voltage period ? Can you give me some instruction and how the protect is implemented during soft start mode ?

3. Gap time
I have read Meng Liu 's question and the answer is that the gap time between two hiccup protection lasts about 7 cycles (of soft start time ) other than the 7 ms recommended in datasheet . However , according to my testing results , the gap time is 25 ms , which does not equal to 7 times 4.7 . I am a little confused . Can you give me some suggestions and guidance ?

4. The vout ripple
As I' m concerned , in FCCM mode the Vout ripple stays the same whatever the load current . However , the ripple varies ab little when I change the load current , which can been seen in the picture below.


The left I_load is 5A, the right is 10A
What's more, the DCM MODE . Base on the dcm theory , the vout ripple should be larger than that of ccm . However , according to my test , the conclusion is inverse . Can you give me some suggestions ?

Thanks a lot for your help and time !