Other Parts Discussed in Thread: TS5A23159
Good day,
My customer is using TPS65070 as a power supply for their current device. The power supply is either from a Li-Ion battery (or Li-Pol), or from USB.
Now they have the new task to run TPS65070 from a Li-SOCL2 battery (for example, SAFT LS 14500) - its voltage is 3.6V. They turned off the charging function in the device, which is planned to be used with a battery.
The problem is that TPS65070 almost never starts-up correctly when powered from the battery. Perhaps the fact is that the maximum current at the start exceeds the limitation 15 mA. Perhaps the problem is with internal logic of the TPS65070. The datasheet says that it is possible to start-up the device at 3.6V.
If they start-up the device from USB firstly, then the device works fine from the battery.
Is it possible to use Li-SOCL2 battery with TPS65070? Is there a schematic solution for this power supply option?
Thank you!
Daria



I attached the part of the schematics and scope shots.