This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Denverton C3508 Solution

Other Parts Discussed in Thread: TPS53622A, TPS53820

Hi 

The CPU is C3508.

The current specification is as below:

Power rail TDC(A) MAX(A)
PVCCP 4 4.5
VNN 4.2 4.5
VCCSRAM 2.5 3

My solution is TPS53622A+CSD95410, but they can't meet Intel CPU spreadsheet Iout accuracy as below:

C3508
 Limit_standard Load(A) Upper Limit(A) Lower Limit(A)
VR Load Tolerance
0% 100.0% 0.00 0.000 0.000
5% 94.0% 0.23 0.446 0.014
10% 47.0% 0.45 0.662 0.239
15% 28.25% 0.68 0.872 0.488
20% 9.5% 0.90 0.986 0.815
25% 8.75% 1.13 1.229 1.031
30% 8.0% 1.35 1.458 1.242
35% 7.50% 1.58 1.699 1.462
40% 7.0% 1.80 1.926 1.674
45% 6.75% 2.03 2.167 1.893
50% 6.5% 2.25 2.396 2.104
55% 6.25% 2.48 2.635 2.325
60% 6.0% 2.70 2.862 2.538
65% 6.00% 2.93 3.106 2.754
70% 6.0% 3.15 3.339 2.961
75% 6.00% 3.38 3.583 3.177
80% 6.0% 3.60 3.816 3.384
85% 6.00% 3.83 4.060 3.600
90% 6.0% 4.05 4.293 3.807
95% 6.00% 4.28 4.537 4.023
100% 6.0% 4.50 4.770 4.365

The Iout is very small.

What solution can meet this Iout accuracy requirement?

Thanks

BR

Hank