Other Parts Discussed in Thread: LM7800,
Hi, support team
My customer has the questions as follow:
LM2940K-15/883 is out of production.
Could you help to find a substitute for me? (Which is in stock)
Thanks so much.
Best regards,
Yuki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Yuki,
LM7800 is the only device with stock that is p2p.
| LM2940C | LM7800 | |
| AEC Q100 | NO | NO |
| Output Options | Fixed Output | Fixed Output |
| Iout (Max) (A) | 1 | 1.5 |
| Vin (Max) (V) | 26 | 30 |
| Vin (Min) (V) | 6 | 7.5 |
| Vout (Max) (V) | 15 | 15 |
| Vout (Min) (V) | 5 | 5 |
| Fixed Output Options (V) | 5, 9, 12, 15 | 5, 12, 15 |
| Enable | NO | NO |
| Power Good | NO | NO |
| Output Capacitor Type | Non-Ceramic | Ceramic, Non-Ceramic |
| PSRR @ 100KHz (dB) | 54 | 48 |
| Noise (uVrms) | 150 | 40 |
| Accuracy (%) | 5 | 3 |
| Vdo (Typ) (mV) | 500 | 2000 |
| Iq (Typ) (mA) | 10 | 6 |
| Thermal Resistance θJA (°C/W) | 23 | 24 |
| Min Package Area (mm2) | 46.5328 | 45.5 |
| Package Type | DDPAK/TO-263, TO-220, TO-220 | DDPAK/TO-263, SOT-223, TO-220 |
Regards,
Prakash L