Other Parts Discussed in Thread: TPS92390
Hi,
I have an application that requires a Li-Ion battery to drive two 12V DC centrifugal fans in parallel, placed at the end of a cable, 600mm from the driver IC. 0.375A per fan, so 0.75A in total. I need to do speed control so I figured using an LED driver would allow me to do analogue dimming, which would reduce the likelihood of EMI radiating from the 600mm long cable.
1. Is it feasible to drive a DC fan from an LED driver, rather than a string of LEDs?
2. Is it feasible that the TPS61500 is capable of driving a 12V/0.75A load, from a 3.5V input?
My 'rough' calculations suggest:
Output Power = 12V * 0.75A = 9W
Assuming 85% Efficiency...
Input Current = (9W / 3.5V) / 0.85 = 3.03A This looks very close to the switching limit of the device?
3. Lastly, should one TPS61500 device not be sufficient, would it be possible to place two TPS61500 CC circuit in parallel, outputs connected together and sharing a common sense resistor?
Thanks!
Robin