Hello,
My situation: Input = [+4,8V / +5,2V] Ouput = [+6V] Consumption = 0,05A
When I try to use webench for these conditions I have a message as: "Design update failed. Duty cycle is lower than the minimum for this device"
Few months ago I was able to use webench with my starting conditions. I don't understand why if I'm changing my input by [3,1V / +3,5V] it is ok.
I saw on another thread that it is important to keep ILIM_SW at 600mA but even at +3,3V I'm stil far from 600mA.
Regards,