This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ25170: Configuration of Pins and Design Questions

Part Number: BQ25170


The device can be configured to charge 1 cell Li-Ion and LiFePO using external pins.  Can the configuration be changed during operation? Any other things I should note?

  • Some useful BQ25170 FAQs

    • How does VIN OVP (input overvoltage protection) function? --- see Data Sheet (SLUSDJ8A) section 7.3.4.1
      • Max input voltage without damaging device is 30 V.
      • Device suspends charging when the input supply is above VIN_OV (6.6 V) until the voltage recovers below the input overvoltage threshold.
      • Device does not have IN-DPM (voltage fold back protection).
    • How do I use the TS pin for Battery temperature monitoring? --- see Data Sheet section 7.3.2.4
      • When TS pin voltage is between VHOT and VCOLD thresholds device will follow standard charge cycle. Thresholds typically correspond to 0°C to 45°C.
      • Voltage at the TS pin outside the operational range results in a recoverable fault. Device suspends charging until battery temperature returns to the acceptable range.
      • High and low thresholds can be modified using series and parallel resistors Rs and Rp between the TS pin and the NTC thermistor.
    • Does the IC have internal thermal regulation?
      • Device monitors internal junction temperature independent of TS battery temperature input pin.
      • Thermal regulation counteracts overheating by limiting charge current when IC temperature exceeds TREG (125°C).
      • Thermal shutdown turns off device if IC temperature exceeds TSHUT (150°C). Device resumes charge when temperature falls below TSHUT falling threshold of 135°C.
    • Does the device have a charge enable pin?
      • The TS pin has the additional functionality of a charge enable pin. Pull TS below VTS_ENZ (50 mV) to disable the charger.
      • Toggling the TS pin will reset the charge cycle and safety timer.
      • The charge disable function of the TS pin provides a means to turn off automatic recharge, which is part of the charging profile by default.
      • System will need to have a method to reenable charging when desired as device does not monitor battery voltage when disabled via the TS pin.
    • Can I change ISET and VSET resistor values during operation?
      • The ISET pin is monitored while charging and changes to R-ISET during operation will immediately change the charge current.
      • The VSET pin is not continuously monitored during charge, once a resistor has been detected the corresponding regulation voltage is set until a reset event occurs.
    • How can I monitor charge current?
      • Voltage developed on the R-ISET resistor maps to output current at a 300 to 1 ratio and can be monitored by an external circuit.
    • What are the functions of the Charging Status (STAT) Pin? --- see Data Sheet section 7.3.3.2
      • STAT is an open drain output with low indicating charge in progress, including automatic recharges. Optional indicator LED will be on during charge.
      • STAT pin will blink at 1 Hz to indicate a fault.
      • STAT pin in high state indicates charge complete or charge disabled.
    • How does the Power Good (/PG) Pin operate? --- see Data Sheet section 7.3.3.1
      • /PG is an open drain output; low state indicates input power is good.
      • Good input power is above VIN_LOWV (3V) and VOUT + 135 mV and below the input overvoltage threshold.
    • Does the device regulate charge current when battery voltage is low?
      • Li-Ion battery voltage less than VBAT_SHORT (2.2 V) and LiFePO4 voltage less than 1.2 V, output current is regulated to IBAT_SHORT (16 mA) for battery short protection.
      • Charge current is limited to the precharge current level when battery voltage is above VBAT_SHORT, but below VBAT_LOWV, 2.8 V for Li-Ion and 2.0 V for LiFePO4.
    • What is the device behavior when no battery is connected? --- see Data Sheet Figure 8-3
      • When no battery is connected to OUT pin the device will quickly cycle in and out of charging with output voltage equal to the VSET regulation voltage.
    • How can the required power dissipation within the IC be reduced?
      • Device acts as a linear regulator, efficiency is improved and power dissipation is reduced the closer Vout is to Vin.
      • Vin will need to be larger than Vout + VDO (dropout voltage) to account for voltage loss internal to the IC.
      • Largest required power dissipation occurs during the beginning of the fast charge phase when battery voltage is low compared to input voltage

    FAQ provided by Garrett Kreger.