Looking for an alternate receiver coil that is more available, some in the EVM User’s Guide and recommended in the Data Sheet are difficult to locate. The coil should work with bq51013B, bq51050B, bq51003, and similar.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
One newer coil we have used in some designs is the Wurth Electronics 760308103215. This coil is in stock at this time with several distributors. It is a larger coil and slightly higher L, this will be a good combination and will give good performance.
Manufacture – Wurth Electronics
Part Number – 760308103215
Dimensions – 48mm x 32mm
Ls – 14.3uH
Output Current Range – 50mA – 1000mA
Application – General 5-V Power Supply