Part Number: TPS7A11
Dear team,
Customer want to use TPS7A11 for 1.1Vin to 0.75Vout/0.11A, and Vpp need to within 1% spec(constant load).
Did we have simulation or calculation can verified device performance?
Regards,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ben,
Please review your bias voltage. You will need some bias voltage headroom at 110mA of load.

I see the requirements are DC only. Depending on your package and min/max junction temperature (and assuming Vbias is not in dropout), this may be able to be met. The EC table has worst case tolerances across line, load and temperature but your requirements are likely inside of these. So I would use the typical datasheet curves.




Thanks,
Stephen